This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/TM4C129XNCZAD: PPP protocol over serial UART

Part Number: TM4C129XNCZAD

Tool/software: TI-RTOS

Hello,

I'm working on a project that needs providing PPP protocol over serial connection UART.

i'm using NDKv2.25 and TM4C129XNCZAD microcontroller.

i can't find any samples with full guidance about this topic, only i got an old example which was integrated with NDK2.00.

it will be great to receive your thoughts

  • Mohamed,

    I asked around, and there isn’t a recent PPP over UART example that I can point you to.  There was an example in older NDK releases, which I think you've found.

    In the most recent TI-RTOS releases there is a “tcpEchoPPP” example.  This example uses PPP over serial USB, and may be useful as a reference(?)

    Regards,
    Scott