Other Parts Discussed in Thread: CDCM6208
Happy New Year All,
I am designing our own board based on the C6678L EVM. We are not planning to use the Hyperlink and we like to use only one CDCM6208 for clocking.
1- Is it safe to not provide MCMCLKP/N (hyperlink_CLKP/N) to pins (W2, Y2)?
2- Can we use the core clock for the PASSCLK and not provide PASSCLKP/N to pins (AJ5, AJ4)...this can be done by setting BM_GPIO = 010
If this is OK, then only clock to the DSP will be: CORECLK, DDRCLK, SRIOSGMIICLK, PCIECLK
I know Ketstone1 has issue with the PLL and hence IBL was introduced and I want to make sure not providing the MCMCLK and EXTERNAL PASSCLK is not an issue!
Regards,
Murad