This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP-L137: omapl137 booting problem with rom id d800k001

Part Number: OMAP-L137

Dear friends,

I am working on 'evm omap l137' and I have problem in booting the DSP code.

Currently I am able to run DSP code using ccs5 and xds510 debugger. But I am not able to boot this code.

I have followed these steps

  • .out file is converted to .bin using AISgentool, selected ROM ID as d800k001 and  selected  configure for evm option.
  • .bin file is loaded in flash using SPI programmer application with option as 'dspais' (which loads the .bin file at 0 location of flash.)

Then after reset I was expecting code to boot and work, but it is not happening.

I have followed same procedure for 6745 dsp based board (with rom id:d800k005) and it is working.

Is there any additional step for omapl137 when compared 6745.

I don't need arm so i have not loaded any arm code.

kindly help me.

regrads

Jagdish