Hello,
I am using 66AK2E05ABDA25 SoC.
According to part number, the Maximum device speed can be 1.25GHz.
There is a register given in datasheet - Device Speed (DEVSPEED) Register
According to this register, Device speed can be 800MHz, 1000MHz, 1200MHz, 1350MHz, 1400MHz.
There is no value as 1250MHz.
So, it creates a doubt that what will be the maximum possible device speed - 1.2GHz or 1.25GHz. (for 66AK2E05ABDA25)
Please clear this doubt.
Thanks and Regards
Tarang Jindal