Other Parts Discussed in Thread: CC2520
Hi all,
I have a hardware interfacing of C5505 USB stick and CC2520 radio. My aim is to sample voice through AIC3204 and send it over radio. After sampling I intend apply speex codec to down convert the stream rate from 64kbps to 5.9kbps.
Now my question is about using ping-pong buffering with AIC3204.
(I have set 48Khz as the sampling frequency in AIC3204. AIC3204_rset( 30, 0x88). I also experimented with 8khz. AIC3204_rset( 30, 0xB0))
We know that ezdsp comes with tests, one of which is about sampling and playback through AIC3204. The code looks something like this
while(1)
{
inputData1 = I2S0_W0_MSW_R;
inputData2 = I2S0_W0_LSW_R;
I2S0_W0_MSW_W = inputData1;
I2S0_W0_LSW_W = inputData2;
}
If I play a song on laptop, give the line-out to AIC line-in and then take AIC line-out over headphone, I can hear a good quality audio.
However, this processing in while loop is inefficient and not suitable to apply ping-pong buffering.
Thus to apply ping-pong buffering, I wrote an ISR routine with GPT through 16Khz timer. I get interrupt every 16Khz, I share it with sampling and playback turn by turn, thus each effectively getting 8Khz. I apply ping-pong buffering here as follows.
interrupt void ticker_ISR(void)
{
if(interruptTurn == SAMPLE_AIC)
{
interruptTurn = PLAYBACK_AIC;
inputData1 = I2S0_W0_MSW_R;
inputData2 = I2S0_W0_LSW_R;
if(encBuffToUse == ENC_PING_BUFFER)
encPingBuffer[indexEncoder] = inputData1;
else
encPongBuffer[indexEncoder] = inputData1;
indexEncoder++;
if(encBuffToUse == ENC_PING_BUFFER)
encPingBuffer[indexEncoder] = inputData2;
else
encPongBuffer[indexEncoder] = inputData2;
indexEncoder++;
if(indexEncoder == (2*FRAME_SIZE))
{
indexEncoder = 0;
//for testing sampling and playback
READY_TO_PLAY = 1;
if(encBuffToUse == ENC_PING_BUFFER)
encBuffToUse = ENC_PONG_BUFFER;
else
encBuffToUse = ENC_PING_BUFFER;
//encodeFrame();
}
}
else
{
interruptTurn = SAMPLE_AIC;
if(READY_TO_PLAY)
{
//for testing sampling and playback
if(encBuffToUse == ENC_PING_BUFFER)
outputData1 = encPongBuffer[indexDecoder];
else
outputData2 = encPingBuffer[indexDecoder];
indexDecoder++;
if(encBuffToUse == ENC_PING_BUFFER)
outputData1 = encPongBuffer[indexDecoder];
else
outputData2 = encPingBuffer[indexDecoder];
indexDecoder++;
I2S0_W0_MSW_W = outputData1;
I2S0_W0_LSW_W = outputData2;
if(indexDecoder == (2*FRAME_SIZE))
{
indexDecoder = 0;
}
}
}
// clearing the timer interrupt bit from IFR0 register
CSL_CPU_REGS->IFR0 = CSL_CPU_REGS->IFR0 & 0xFFEF;
//Clearing TIAF register bit corresponding to Timer0
(*iafrReg) = (*iafrReg)| (0x0001) ;
}
If you have noticed in this program, I am not applying encoding or decoding, but simply passing the buffers to playback so that sampling and playback can happen simultaneously. This is a test of ping-pong buffering before applying codec. This should sample voice from line-in and playback voice on line-out.
However, when I test this through line-in (laptop) and line-out (headphone) for a song or voice sample, I get very poor quality audio.I can recognize the song being played but pitch gets down suddenly. This is worse because I have not even applied codec.
And this is not because of low sampling frequency of AIC3204 (48Khz or 8Khz) as the while loop program gives good quality output. This is also not because of low sampling frequency of GPT (8khz) as I tried with 48Khz sampling as well.
Is this because of GPT overhead? How should I go about doing this then?
Or is this because of some AIC3204 setting?
Awaiting early reply.
Thanks in advance.
Vijay