This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM385: Facing issue with streaming video

Part Number: DM385


Hi,


We are using custom dm385 board, with EZSDK. linux kernel 2.6.37. On source side we have hdmi input which is connected a media player. on sink side we have hdmi out which connect to display. Source and sink are connected using p2p. When started streaming display goes blank. For streaming omx_videsrc is used.
 

VPSS logs on Source side.

SysLink module created on Date:Jan  3 2017 Time:18:47:59
PM: Adding info for No Bus:syslinkipc_Osal
PM: Adding info for No Bus:syslinkipc_Ipc
PM: Adding info for No Bus:syslinkipc_ProcMgr
PM: Adding info for No Bus:syslinkipc_Notify
PM: Adding info for No Bus:syslinkipc_MultiProc
PM: Adding info for No Bus:syslinkipc_NameServer
PM: Adding info for No Bus:syslinkipc_SharedRegion
PM: Adding info for No Bus:syslinkipc_HeapBufMP
PM: Adding info for No Bus:syslinkipc_HeapMemMP
PM: Adding info for No Bus:syslinkipc_ListMP
PM: Adding info for No Bus:syslinkipc_GateMP
PM: Adding info for No Bus:syslinkipc_MessageQ
PM: Adding info for No Bus:syslinkipc_SyslinkMemMgr
PM: Adding info for No Bus:syslinkipc_ClientNotifyMgr
PM: Adding info for No Bus:syslinkipc_FrameQBufMgr
PM: Adding info for No Bus:syslinkipc_FrameQ
PM: Adding info for No Bus:syslinkipc_RingIO
PM: Adding info for No Bus:syslinkipc_RingIOShm
VPSS_CORE : core init
VPSS_CORE : cpu version 0x81400081
VPSS_SHRBUF: sbuf init
VPSS_SHRBUF: map 0xafb00000 to 0xccc00000 with size 2097152
VPSS_FVID2: fvid2 init
VPSS_FVID2: Handshake...
VPSS_SHRBUF: FOUND 0xafb00000, end 0xafd00000, map vir 0xccc00000 size 4096
VPSS_SHRBUF: free mem paddr 0xafb00000 vaddr 0xccc00000 size 4096
VPSS_FVID2: M3 firmware version 0x1000143 is newer,driver may not work properly.
VPSS_SYSTEM: enter system init
VPSS_SHRBUF: FOUND 0xafb00000, end 0xafd00000, map vir 0xccc00000 size 4096
VPSS_SHRBUF: FOUND 0xafb01000, end 0xafd00000, map vir 0xccc01000 size 4096
VPSS_FVID2: Fvid2 handle 0x8ee0c420 with notifyno 10 within 2 ms
VPSS_FVID2: send control with cmd 0x10080002
VPSS_FVID2: control event 0x10080002 return 0 within 0 ms.
VPSS_DCTRL: dctrl init
VPSS_SHRBUF: FOUND 0xafb02000, end 0xafd00000, map vir 0xccc02000 size 4096
VPSS_SHRBUF: FOUND 0xafb03000, end 0xafd00000, map vir 0xccc03000 size 4096
VPSS_FVID2: Fvid2 handle 0x8ee0c440 with notifyno 11 within 0 ms
VPSS_DCTRL: mode hdmi:1080p-60
VPSS_FVID2: send control with cmd 0x10040003
VPSS_FVID2: control event 0x10040003 return 0 within 0 ms.
VPSS_DCTRL: HDCOMP timing changed to match HDMI
VPSS_FVID2: send control with cmd 0x1004001c
VPSS_FVID2: control event 0x1004001c return 0 within 0 ms.
VPSS_SYSTEM: enter set pll 148500KHz for VENC 2
VPSS_SYSTEM: request clk 1485000000Hz
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x10040019
VPSS_FVID2: control event 0x10040019 return 0 within 0 ms.
VPSS_GRPX : grpx init
VPSS_SHRBUF: FOUND 0xafb04000, end 0xafd00000, map vir 0xccc04000 size 4096
VPSS_VIDEO: video init
VPSS_SHRBUF: FOUND 0xafb05000, end 0xafd00000, map vir 0xccc05000 size 8192
VPSS_CAPTURE: cap init
VPSS_SHRBUF: FOUND 0xafb07000, end 0xafd00000, map vir 0xccc07000 size 49152
VPSS_SHRBUF: sharing buffer used 77824 byte, left 2019328 bytes
VPSS_GRPX : (0)- get resolution.
VPSS_DCTRL: enter get output format
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_GRPX : (0)- get resolution.
VPSS_DCTRL: enter get output format
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 2 ms.
VPSS_GRPX : (0)- get resolution.
VPSS_DCTRL: enter get output format
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_GRPX : (0)- get region params.
VPSS_GRPX : (0)- get sc params.
VPSS_GRPX : (0)- get resolution.
VPSS_DCTRL: enter get output format
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_GRPX : (0) - get timing
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_GRPX : (1)- get resolution.
VPSS_DCTRL: enter get output format
VPSS_GRPX : (2)- get resolution.
VPSS_DCTRL: enter get output format
VPSS_GRPX : (0)- apply changes into FVID2_FRAME.
VPSS_GRPX : (0)- set format bpp 32 df 4104, pitch 7680.
VPSS_GRPX : (0)- get region params.
VPSS_GRPX : (0)- set region params.
VPSS_GRPX : (0)- add buffer 0x87700000
VPSS_GRPX : (0)- apply changes into FVID2_FRAME.
PM: Adding info for No Bus:fb0
PM: Adding info for No Bus:fb1
PM: Adding info for No Bus:fb2
HDMI W1 rev 4.0
HDMI CEC Spec version 1.2
HDCP initialized
PM: Adding info for No Bus:TI81XX_HDMI
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x10040004
VPSS_FVID2: control event 0x10040004 return 0 within 0 ms.
VPSS_SYSTEM: enter set pll 148500KHz for VENC 3
VPSS_SYSTEM: request clk 1485000000Hz
hdmi: Enter HDMI_W1_StopVideoFrame()
hdmi: *** Set PHY power mode to 1
hdmi: *** Set PHY power mode to 2
I2C No Ack

HDMI failed to read E-EDID
hdmi: Enter HDMI_W1_GlobalInitVars()
hdmi: Enter HDMI_Core_GlobalInitVars()
hdmi: Enter HDMI_W1_ConfigVideoResolutionTiming()
hdmi: Enter HDMI_W1_ConfigVideoInterface()
hdmi: Enter DSS_HDMI_CORE_SW_RESET_ASSERT ()
hdmi: Enter DSS_HDMI_CORE_POWER_DOWN_DISABLE()
hdmi: Enter DSS_HDMI_CORE_SW_RESET_RELEASE()
hdmi: Enter HDMI_W1_StartVideoFrame  ()
hdmi: Irqenable 60000011
hdmi: 40 hpd
Compat-wireless backport release: ol_r8.a6.06
Backport based on wl18xx.git ol_r8.a6.02
compat.git: wl18xx.git
In set power wlan!!
powering on the chip!!|nId to be disabled:1, venc mask:1
VPSS_DCTRL: enter venc disable
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x1004001b
VPSS_FVID2: control event 0x1004001b return 0 within 0 ms.
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 0 ms.
hdmi: Enter DSS_HDMI_CORE_SW_RESET_ASSERT ()
hdmi: Enter HDMI_W1_StopVideoFrame()
hdmi: *** Set PHY power mode to 0
hdmi: *** Set PHY power mode to 0
VPSS_FVID2: send control with cmd 0x1004001a
VPSS_FVID2: control event 0x1004001a return 0 within 2 ms.
VPSS_FVID2: send control with cmd 0x10040019
VPSS_FVID2: control event 0x10040019 return 0 within 0 ms.
hdmi: Enter HDMI_W1_StopVideoFrame()
hdmi: *** Set PHY power mode to 1
hdmi: *** Set PHY power mode to 2
PM: Adding info for platform:wl18xx
In set power wlan!!
powering off the chip!!|n
PM: Adding info for platform:regulatory.0
cfg80211: Calling CRDA to update world regulatory domain
I2C No Ack

HDMI failed to read E-EDID
hdmi: Enter HDMI_W1_GlobalInitVars()
hdmi: Enter HDMI_Core_GlobalInitVars()
hdmi: Enter HDMI_W1_ConfigVideoResolutionTiming()
hdmi: Enter HDMI_W1_ConfigVideoInterface()
hdmi: Enter DSS_HDMI_CORE_SW_RESET_ASSERT ()
hdmi: Enter DSS_HDMI_CORE_POWER_DOWN_DISABLE()
hdmi: Enter DSS_HDMI_CORE_SW_RESET_RELEASE()
hdmi: Enter HDMI_W1_StartVideoFrame  ()
hdmi: Irqenable 60000011
hdmi: 40 hpd
hdmi: Enter DSS_HDMI_CORE_SW_RESET_ASSERT ()
hdmi: Enter HDMI_W1_StopVideoFrame()
hdmi: *** Set PHY power mode to 0
hdmi: *** Set PHY power mode to 0
hdmi: Enter HDMI_W1_StopVideoFrame()
hdmi: *** Set PHY power mode to 1
hdmi: *** Set PHY power mode to 2
cfg80211: World regulatory domain updated:
cfg80211:   (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp)
cfg80211:   (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
cfg80211:   (2457000 KHz - 2482000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
cfg80211:   (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
cfg80211:   (5170000 KHz - 5250000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
cfg80211:   (5735000 KHz - 5835000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
wlcore: wl18xx driver version: ol_r8.a6.02
PM: Adding info for No Bus:wl18xx
PM: Removing info for No Bus:wl18xx
In set power wlan!!
powering on the chip!!|nI2C No Ack

HDMI failed to read E-EDID
hdmi: Enter HDMI_W1_GlobalInitVars()
wlcore: wl18xx HW: RDL 2, 1857 MIMO, PG 2.2 (ROM 0x11)
In set power wlan!!
powering off the chip!!|n
PM: Adding info for No Bus:wl18xx
PM: Removing info for No Bus:wl18xx
PM: Adding info for No Bus:phy0
PM: Adding info for No Bus:rfkill0
PM: Adding info for No Bus:wlan0
wlcore: loaded
wlcore: driver version: ol_r8.a6.02
wlcore: timestamp: Wed Oct 19 19:06:34 2016
hdmi: Enter HDMI_Core_GlobalInitVars()
hdmi: Enter HDMI_W1_ConfigVideoResolutionTiming()
hdmi: Enter HDMI_W1_ConfigVideoInterface()
hdmi: Enter DSS_HDMI_CORE_SW_RESET_ASSERT ()
hdmi: Enter DSS_HDMI_CORE_POWER_DOWN_DISABLE()
hdmi: Enter DSS_HDMI_CORE_SW_RESET_RELEASE()
hdmi: Enter HDMI_W1_StartVideoFrame  ()
hdmi: Irqenable 60000011
hdmi: 40 hpd

Omx hangs after sending command, with log

sil9135:Detecting Video