Part Number: 66AK2E05
Hello,
As per the hardware design guide of K2E device,
The VID values is driven out using all VCNTL pins once the POR is released. but according to device manual, the configuration pins are sampled at nResetfull de-assertion.
The AVSIFSEL are also the configuration pins which sampled at nRESETFULL de-assertion. AVSIFSEL decides that which AVS interface mode is selected.
so, how device provides VID values on VCNTL pins immediate after POR is released. (As it is also mentioned that nRESETFULL should be de-asserted after POR de-assertion.
is my understanding regarding VID value generation sequence is correct? If not, please let me know that at what instant (after power up or nReset or nPOR or nRESETFULL ) device provides the VID values on VCNTL pins.
if SoC provides VID values after nPOR then how device knows that which AVS mode is selected ?
Thanks and Regards
Tarang Jindal