Other Parts Discussed in Thread: OMAP3503
We've recently started prototyping with a Gumstix Overo (OMAP3503) and have now discovered we may need to add a mini PCI-E device (with USB pins 36,38 N/C). I guessed that there would be a simple bridge chip that would allow us to use the USB host as the interface to the processor but cannot find anything appropriate. I know of at least one product that must do this, the Ubiquiti SR71-USB, as it uses the Atheros AR9280 (with PCI-E IF) but not surprisingly have had no response from them.
I'm hoping someone may have some experience with PCI-E / OMAP35xx relations they're willing to share? I'm not particularly fond of having to change processor at this point.
Edit: I've received a Ubiquiti SR71-USB and not surprisingly it does not use the advertised chipset. Support has confirmed this but not commented as to whether they will fix their datasheets.