This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSICE3359: Writing EtherCAT Master code to flash memory

Part Number: TMDSICE3359


Hi

I would like to flash the ethercat master code onto TMDSICE3359 so that whenever the board powers up, it is in ethercat master straight away, without the need for me to run the ethercat master code every time.

Also, I would like the default code (and .hex file) which comes with the TMDSICE3359, out of the box. This code displays "IASDK 1.1.0.5 EtherCAT_Demo" on the LED screen.

Thanks.