This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XEVMK2EX: How EVM is meeting clock jitter requirements of K2E SoC

Part Number: XEVMK2EX

Hello, 

According to SoC, Random Jitter requirement for most of the interfaces is below 4ps RMS. 

EVM has used CDCM6208V1RGZT clock generator to source the clocks for SoC. The ref clock for this clock source is a 25MHz oscillator. 

According to 25MHz Osc specs, osc has 5ps RMS jitter.  

if EVM is using a 5ps RMS noisy ref clock osc. and clock source is used in synthesized mode, so, how are you meeting the jitter requirement of SoC with this set up.

Thanks and Regards

Tarang Jindal