Tool/software: TI-RTOS
How to run sys/bios example after uboot on TCI6636K2H ev board ?
I would like to run simple example after uboot without gel file.
- I don't want to use default gel file ( xtcievmk2x_arm.gel )
- Import hello_TCI6638K2K_CortexA from ccs resource browser and build & make bin file
- mkimage -A arm -T kernel -C none -a 0x80000000 -e 0x800050ec -d hello_TCI6638K2K_CortexA.bin hello_TCI6638K2K_CortexA _for_uboot.bin
- Power on TCI6636K2H ev board.
- Download hello_TCI6638K2K_CortexA _for_uboot.bin @0x80000000
- bootm 0x80000000
but It is not working
Please let me know what is correct way to run sys/bios example after uboot.
U-Boot SPL 2016.09-rc2 (Jan 09 2017 - 20:44:29)
Trying to boot from SPI
U-Boot 2013.01-00004-g0c2f8a2 (Aug 16 2013 - 19:04:15)
I2C: ready
DRAM: 2 GiB
NAND: 512 MiB
Net: TCI6638_EMAC
Warning: TCI6638_EMAC using MAC address from net device
, TCI6638_EMAC1
Hit any key to stop autoboot: 0
TCI6638 EVM #
TCI6638 EVM # loadb 0x80000000
## Ready for binary (kermit) download to 0x80000000 at 115200 bps...
## Total Size = 0x0001e9b0 = 125360 Bytes
## Start Addr = 0x80000000
TCI6638 EVM # bootm 0x80000000
## Booting kernel from Legacy Image at 80000000 ...
Image Name:
Created: 2017-01-09 8:57:33 UTC
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 125296 Bytes = 122.4 KiB
Load Address: 80000000
Entry Point: 800050ec
Verifying Checksum ... OK
XIP Kernel Image ... OK
OK
Starting kernel ...