Other Parts Discussed in Thread: TIDM-TM4C129XGATEWAY
Tool/software: TI-RTOS
Hi,
I am using ccs v6.2 with tm4c1294xl launchpad, cc3100bp.
I want to enable both wifi and emac on my device, I success fully connected to wifi and it was working in the same main going to initialize the emac also but when I am calling anything from the EMAC class of tirtos it was not building instead giving an errors
**#10010 errors encountered during linking; "newproject.out" not built
** #10234-D unresolved symbols remain and
** unresolved symbol SemPost, first referenced in C:/ti/tirex-content/tirtos_tivac_2_16_00_08/products/tidrivers_tivac_2_16_00_08/packages/ti/drivers/lib/drivers_tivaware.aem4f<EMACSnow.oem4f>
Building Console prints:
<xxx Till here no errors xxxx>
<Linking>
undefined first referenced
symbol in file
--------- ----------------
SemPost C:/ti/tirex-content/tirtos_tivac_2_16_00_08/products/tidrivers_tivac_2_16_00_08/packages/ti/drivers/lib/drivers_tivaware.aem4f<EMACSnow.oem4f>
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "Kiko_Point.out" not built
>> Compilation failure
makefile:162: recipe for target 'Kiko_Point.out' failed
gmake: *** [Kiko_Point.out] Error 1
gmake: Target 'all' not remade because of errors.
**** Build Finished ****
I has not calling any of wifi init or wifi related functions, if I not call any EMAC class functions it was building and running fine, but I have to use the EMAC_init() of this class to initialize emac. As well I check with tirtos provided example project also all the includes and header used properly.
So, can you help me to resolve these errors.
Thanks,
Regards,
Raghu DS.