Part Number: AM3352
Hi Sir
this is my /proc/cpuinfo information
processor : 0
model name : ARMv7 Processor rev 2 (v7l)
BogoMIPS : 298.80
Features : swp half thumb fastmult vfp edsp thumbee neon vfpv3 tls vfpd32
CPU implementer : 0x41
CPU architecture: 7
CPU variant : 0x3
CPU part : 0xc08
CPU revision : 2
Hardware : Generic AM33XX (Flattened Device Tree)
Revision : 0000
Serial : 0000000000000000
base on the file , I assume that the cpu of my custom board is running at 300MHz
How can I do to make it run at 600MHz
Best Regard
Vic