Part Number: AM3358
Other Parts Discussed in Thread: AM3352, TPS65910
Tool/software: Linux
Hello,
A couple of days ago I switched from processor-sdk-linux-am335x-evm-02.00.02.11 to processor-sdk-linux-am335x-evm-03.02.00.05 in order to check if a problem in a driver for SC16IS7XX (I2c to UART bridge) in krenel 4.1 is fixed in kernel 4.4.
When I first prepared an SD card and installed the pre-built images from SDK, everything went smooth.
The problem is that when I rebuilt the original am335x-evmsk.dts file (by typing: make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- am335x-evmsk.dtb in the SDK home directory) the result was a 41KB dtb file, different from the original 40.9KB dtb file, and when I loaded it to the SD card the result was an error, as can be seen in the following log:
U-Boot SPL 2016.05-g6c5519b6fc (Dec 14 2016 - 19:14:27)
Trying to boot from MMC1
reading args
spl_load_image_fat_os: error reading image args, err - -1
reading u-boot.img
reading u-boot.img
reading u-boot.img
reading u-boot.img
U-Boot 2016.05-g6c5519b6fc (Dec 14 2016 - 19:14:27 -0500)
CPU : AM335X-GP rev 2.1
Model: TI AM335x EVM-SK
Watchdog enabled
DRAM: 256 MiB
NAND: 0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
reading uboot.env
** Unable to read "uboot.env" from mmc0:1 **
Using default environment
<ethaddr> not set. Validating first E-fuse MAC
Net: Could not get PHY for ethernet@4a100000: addr 0
eth0: ethernet@4a100000
Warning: usb_ether MAC addresses don't match:
Address in SROM is de:ad:be:ef:00:01
Address in environment is 88:4a:ea:ca:f6:63
, eth1: usb_ether
Press SPACE to abort autoboot in 2 seconds
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
reading boot.scr
** Unable to read file boot.scr **
reading uEnv.txt
** Unable to read file uEnv.txt **
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:1...
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
3467136 bytes read in 282 ms (11.7 MiB/s)
36668 bytes read in 36 ms (994.1 KiB/s)
Kernel image @ 0x82000000 [ 0x000000 - 0x34e780 ]
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8ef1a000, end 8ef25f3b ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 4.4.32-gadde2ca9f8 (yehuda@EGM) (gcc version 4.8.4 (Ubuntu/Linaro 4.8.4-2ubuntu1~14.04.1) ) #1 PREEMPT Tue Jan 10 19:18:28 IST 2017
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine model: TI AM335x EVM-SK
[ 0.000000] cma: Reserved 48 MiB at 0x8b800000
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES2.1 (sgx neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 64960
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=PARTUUID=0004114a-02 rw rootfstype=ext4 rootwait
[ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.000000] Memory: 200400K/262144K available (6551K kernel code, 318K rwdata, 2348K rodata, 268K init, 266K bss, 12592K reserved, 49152K cma-reserved, 0K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xd0800000 - 0xff800000 ( 752 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc08b8fd4 (8900 kB)
[ 0.000000] .init : 0xc08b9000 - 0xc08fc000 ( 268 kB)
[ 0.000000] .data : 0xc08fc000 - 0xc094b8d8 ( 319 kB)
[ 0.000000] .bss : 0xc094b8d8 - 0xc098e0f0 ( 267 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Build-time adjustment of leaf fanout to 32.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[ 0.000016] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
[ 0.000038] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
[ 0.000049] OMAP clocksource: timer1 at 24000000 Hz
[ 0.000212] clocksource_probe: no matching clocksources found
[ 0.000404] Console: colour dummy device 80x30
[ 0.000434] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.000441] This ensures that you still see kernel messages. Please
[ 0.000447] update your kernel commandline.
[ 0.000467] Calibrating delay loop... 795.44 BogoMIPS (lpj=3977216)
[ 0.089055] pid_max: default: 32768 minimum: 301
[ 0.089179] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.089192] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.089915] Initializing cgroup subsys io
[ 0.089948] Initializing cgroup subsys memory
[ 0.089989] Initializing cgroup subsys devices
[ 0.090006] Initializing cgroup subsys freezer
[ 0.090021] Initializing cgroup subsys perf_event
[ 0.090034] Initializing cgroup subsys pids
[ 0.090062] CPU: Testing write buffer coherency: ok
[ 0.090494] Setting up static identity map for 0x80008200 - 0x80008258
[ 0.092704] devtmpfs: initialized
[ 0.104487] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.119587] omap_hwmod: debugss: _wait_target_disable failed
[ 0.174872] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.178957] pinctrl core: initialized pinctrl subsystem
[ 0.180524] NET: Registered protocol family 16
[ 0.182820] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.209054] cpuidle: using governor ladder
[ 0.239041] cpuidle: using governor menu
[ 0.243633] OMAP GPIO hardware version 0.1
[ 0.254808] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.297690] edma 49000000.edma: TI EDMA DMA engine driver
[ 0.302426] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c0_pins, deferring probe
[ 0.302483] omap_i2c 4802a000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c1_pins, deferring probe
[ 0.302606] media: Linux media interface: v0.10
[ 0.302673] Linux video capture interface: v2.00
[ 0.302727] pps_core: LinuxPPS API ver. 1 registered
[ 0.302735] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.302766] PTP clock support registered
[ 0.302827] EDAC MC: Ver: 3.0.0
[ 0.304051] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 0.304407] Advanced Linux Sound Architecture Driver Initialized.
[ 0.305633] clocksource: Switched to clocksource timer1
[ 0.316841] NET: Registered protocol family 2
[ 0.317663] TCP established hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.317704] TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.317732] TCP: Hash tables configured (established 2048 bind 2048)
[ 0.317819] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.317839] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.317996] NET: Registered protocol family 1
[ 0.318442] RPC: Registered named UNIX socket transport module.
[ 0.318459] RPC: Registered udp transport module.
[ 0.318465] RPC: Registered tcp transport module.
[ 0.318472] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.319454] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
[ 0.321527] futex hash table entries: 256 (order: -1, 3072 bytes)
[ 0.329910] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.330876] NFS: Registering the id_resolver key type
[ 0.330958] Key type id_resolver registered
[ 0.330968] Key type id_legacy registered
[ 0.331042] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.334889] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247)
[ 0.334926] io scheduler noop registered
[ 0.334940] io scheduler deadline registered
[ 0.335097] io scheduler cfq registered (default)
[ 0.336857] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[ 0.401123] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[ 0.405458] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 158, base_baud = 3000000) is a 8250
[ 1.011946] console [ttyS0] enabled
[ 1.016830] 48022000.serial: ttyS1 at MMIO 0x48022000 (irq = 159, base_baud = 3000000) is a 8250
[ 1.026969] 48024000.serial: ttyS2 at MMIO 0x48024000 (irq = 160, base_baud = 3000000) is a 8250
[ 1.037009] 481a6000.serial: ttyS3 at MMIO 0x481a6000 (irq = 161, base_baud = 3000000) is a 8250
[ 1.047063] 481a8000.serial: ttyS4 at MMIO 0x481a8000 (irq = 162, base_baud = 3000000) is a 8250
[ 1.057116] 481aa000.serial: ttyS5 at MMIO 0x481aa000 (irq = 163, base_baud = 3000000) is a 8250
[ 1.067179] [drm] Initialized drm 1.1.0 20060810
[ 1.073806] tilcdc 4830e000.lcdc: no encoders/connectors found
[ 1.087449] loop: module loaded
[ 1.093199] libphy: Fixed MDIO Bus: probed
[ 1.155719] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6
[ 1.161862] davinci_mdio 4a101000.mdio: detected phy mask fffffffd
[ 1.169095] libphy: 4a101000.mdio: probed
[ 1.173133] davinci_mdio 4a101000.mdio: phy[1]: device 4a101000.mdio:01, driver Atheros 8031 ethernet
[ 1.183266] cpsw 4a100000.ethernet: Detected MACID = 88:4a:ea:ca:f6:61
[ 1.190082] cpsw 4a100000.ethernet: cpts: overflow check period 850
[ 1.197324] cpsw 4a100000.ethernet: cpsw: Detected MACID = 88:4a:ea:ca:f6:63
[ 1.206068] mousedev: PS/2 mouse device common for all mice
[ 1.212353] i2c /dev entries driver
[ 1.217422] cpuidle: enable-method property 'ti,am3352' found operations
[ 1.224997] omap_hsmmc 48060000.mmc: Got CD GPIO
[ 1.286376] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.295501] NET: Registered protocol family 10
[ 1.301687] sit: IPv6 over IPv4 tunneling driver
[ 1.307304] NET: Registered protocol family 17
[ 1.312119] Key type dns_resolver registered
[ 1.316762] omap_voltage_late_init: Voltage driver support not added
[ 1.345871] tps65910 0-002d: No interrupt support, no core IRQ
[ 1.377347] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[ 1.396632] omap_i2c 4802a000.i2c: bus 1 rev0.11 at 400 kHz
[ 1.402991] omap_hsmmc 48060000.mmc: Got CD GPIO
[ 1.408158] vmmc: supplied by vbat
[ 1.482758] mmc0: host does not support reading read-only switch, assuming write-enable
[ 1.491190] vdd_mpu: supplied by vbat
[ 1.496750] hctosys: unable to open rtc device (rtc0)
[ 1.502011] mmc0: new high speed SDHC card at address 59b4
[ 1.511462] lis3_reg: disabling
[ 1.515815] mmcblk0: mmc0:59b4 USDU1 7.51 GiB
[ 1.521343] ALSA device list:
[ 1.524484] mmcblk0: p1 p2
[ 1.527648] No soundcards found.
[ 1.570124] mmc1: MAN_BKOPS_EN bit is not set
[ 1.580388] mmc1: new high speed MMC card at address 0001
[ 1.588382] mmcblk1: mmc1:0001 MMC04G 3.60 GiB
[ 1.593241] mmcblk1boot0: mmc1:0001 MMC04G partition 1 16.0 MiB
[ 1.599612] mmcblk1boot1: mmc1:0001 MMC04G partition 2 16.0 MiB
[ 2.085288] EXT4-fs (mmcblk0p2): recovery complete
[ 2.093671] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 2.102006] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 2.116676] devtmpfs: mounted
[ 2.120844] Freeing unused kernel memory: 268K (c08b9000 - c08fc000)
[ 2.127310] This architecture does not have kernel memory protection.
[ 2.435814] systemd[1]: System time before build time, advancing clock.
[ 2.500236] random: systemd: uninitialized urandom read (16 bytes read, 23 bits of entropy available)
[ 2.516262] random: systemd: uninitialized urandom read (16 bytes read, 23 bits of entropy available)
[ 2.539794] systemd[1]: systemd 229 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT +GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN)
[ 2.558913] systemd[1]: Detected architecture arm.
Welcome to Arago 2016.10!
[ 2.587292] systemd[1]: Set hostname to <am335x-evm>.
[ 2.697911] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 26 bits of entropy available)
[ 2.717132] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 26 bits of entropy available)
[ 2.733646] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 27 bits of entropy available)
[ 2.749787] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 27 bits of entropy available)
[ 2.775569] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 28 bits of entropy available)
[ 2.879452] random: systemd: uninitialized urandom read (16 bytes read, 32 bits of entropy available)
[ 2.889645] random: systemd: uninitialized urandom read (16 bytes read, 32 bits of entropy available)
[ 2.900753] random: systemd: uninitialized urandom read (16 bytes read, 32 bits of entropy available)
[ 3.278622] systemd[1]: [/lib/systemd/system/gadget-init.service:15] Unknown lvalue 'ExecStopPre' in section 'Service'
[ 3.597751] systemd[1]: sysinit.target: Found ordering cycle on sysinit.target/start
[ 3.605599] systemd[1]: sysinit.target: Found dependency on alignment.service/start
[ 3.613593] systemd[1]: sysinit.target: Found dependency on basic.target/start
[ 3.620918] systemd[1]: sysinit.target: Found dependency on sysinit.target/start
[ 3.628396] systemd[1]: sysinit.target: Breaking ordering cycle by deleting job alignment.service/start
[ 3.637878] systemd[1]: alignment.service: Job alignment.service/start deleted to break ordering cycle starting with sysinit.target/start
[ SKIP ] Ordering cycle found, skipping alignment.service
[ 3.686602] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 3.716509] systemd[1]: Listening on Syslog Socket.
[ OK ] Listening on Syslog Socket.
[ 3.746101] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 3.776352] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe.
[ OK ] Listening on /dev/initctl Compatibility Named Pipe.
[ 3.806446] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 3.836399] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 3.866411] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password Requests to Wall Directory Watch.
[ 3.897550] systemd[1]: Created slice System Slice.
[ OK ] Created slice System Slice.
[ 3.939255] systemd[1]: Mounting Temporary Directory...
Mounting Temporary Directory...
[ 3.991141] systemd[1]: Starting Load Kernel Modules...
Starting Load Kernel Modules...
[ 4.044878] cryptodev: driver 1.8 loaded.
[ 4.051367] systemd[1]: Created slice system-getty.slice.
[ OK ] Created slice system-getty.slice.
[ 4.092317] systemd[1]: Starting Create list of required static device nodes for the current kernel...
Starting Create list of required st... nodes for the current kernel...
[ 4.151657] systemd[1]: Mounting Debug File System...
Mounting Debug File System...
[ 4.196324] systemd[1]: Reached target Slices.
[ OK ] Reached target Slices.
[ 4.228083] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ 4.256599] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 4.286849] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 4.330538] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 4.377323] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems...
[ 4.445189] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[ 4.451955] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password Requests to Console Directory Watch.
[ 4.516403] systemd[1]: Reached target Paths.
[ OK ] Reached target Paths.
[ 4.546377] systemd[1]: Reached target Swap.
[ OK ] Reached target Swap.
[ 4.556727] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 4.602272] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 4.671719] systemd[1]: Starting Setup Virtual Console...
Starting Setup Virtual Console...
[ 4.785389] systemd[1]: Mounted POSIX Message Queue File System.
[ OK ] Mounted POSIX Message Queue File System.
[ 4.836459] systemd[1]: Mounted Debug File System.
[ OK ] Mounted Debug File System.
[ 4.856408] systemd[1]: Mounted Temporary Directory.
[ OK ] Mounted Temporary Directory.
[ 4.889049] systemd[1]: Started Load Kernel Modules.
[ OK ] Started Load Kernel Modules.
[ 4.908285] systemd[1]: Started Create list of required static device nodes for the current kernel.
[ OK ] Started Create list of required sta...ce nodes for the current kernel.
[ 4.958699] systemd[1]: Started Remount Root and Kernel File Systems.
[ OK ] Started Remount Root and Kernel File Systems.
[ 4.998877] systemd[1]: Started Setup Virtual Console.
[ OK ] Started Setup Virtual Console.
[ 6.147001] systemd[1]: Starting udev Coldplug all Devices...
Starting udev Coldplug all Devices...
[ 6.191617] systemd[1]: Starting Create Static Device Nodes in /dev...
Starting Create Static Device Nodes in /dev...
[ 6.271389] systemd[1]: Starting Apply Kernel Variables...
Starting Apply Kernel Variables...
[ 6.401646] systemd[1]: Started Create Static Device Nodes in /dev.
[ OK ] Started Create Static Device Nodes in /dev.
[ 6.468516] systemd[1]: Started Apply Kernel Variables.
[ OK ] Started Apply Kernel Variables.
[ 7.310892] systemd[1]: Starting udev Kernel Device Manager...
Starting udev Kernel Device Manager...
[ 7.366294] systemd[1]: Reached target Local File Systems (Pre).
[ OK ] Reached target Local File Systems (Pre).
[ 7.424072] systemd[1]: Mounting /media/ram...
Mounting /media/ram...
[ 7.500614] systemd[1]: Mounting /var/volatile...
Mounting /var/volatile...
[ 7.641536] systemd[1]: Mounted /var/volatile.
[ OK ] Mounted /var/volatile.
[ 7.676508] systemd[1]: Mounted /media/ram.
[ OK ] Mounted /media/ram.
[ 7.789511] systemd[1]: Started udev Kernel Device Manager.
[ OK ] Started udev Kernel Device Manager.
[ 8.845505] systemd[1]: Starting Load/Save Random Seed...
Starting Load/Save Random Seed...
[ 8.996424] systemd[1]: Reached target Local File Systems.
[ OK ] Reached target Local File Systems.
[ 9.058943] systemd[1]: Started Load/Save Random Seed.
[ OK ] Started Load/Save Random Seed.
[ 9.233636] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 9.315062] omap_rtc 44e3e000.rtc: rtc core: registered 44e3e000.rtc as rtc0
[ 9.388000] 47401300.usb-phy supply vcc not found, using dummy regulator
[ 9.464312] 47401b00.usb-phy supply vcc not found, using dummy regulator
[ 9.588561] systemd[1]: Started udev Coldplug all Devices.
[ OK ] Started udev Coldplug all Devices.
[ 9.730404] systemd[1]: Found device /dev/ttyS0.
[ OK ] Found device /dev/ttyS0.
[ 9.962808] omap_rng 48310000.rng: OMAP Random Number Generator ver. 20
[ 10.498054] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
[ 10.533700] systemd[1]: Found device /dev/ttyS3.
[ OK ] Found device /dev/ttyS3.
[ 10.837505] remoteproc0: wkup_m3 is available
[ 10.841997] remoteproc0: Note: remoteproc is still under development and considered experimental.
[ 10.957815] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
[ 11.004960] remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 11.628628] ti-pruss 4a300000.pruss: creating PRU cores and other child platform devices
[ 11.667598] remoteproc0: powering up wkup_m3
[ 11.673237] remoteproc0: Booting fw image am335x-pm-firmware.elf, size 217280
[ 11.703172] irq: no irq domain found for /ocp/pruss@4a300000/intc@4a320000 !
[ 11.807038] irq: no irq domain found for /ocp/pruss@4a300000/intc@4a320000 !
[ 11.826646] remoteproc0: remote processor wkup_m3 is now up
[ 11.826677] wkup_m3_ipc 44e11324.wkup_m3_ipc: CM3 Firmware Version = 0x192
[ 11.929648] [drm] Initialized pvr 1.14.3699939 20110701 on minor 0
[ 11.974951] remoteproc1: 4a334000.pru0 is available
[ 11.984144] PM: bootloader does not support rtc-only!
[ 12.038312] systemd[1]: dev-disk-by\x2dpath-platform\x2d481d8000.mmc.device: Dev dev-disk-by\x2dpath-platform\x2d481d8000.mmc.device appeared twice with different sysfs paths /sys/devices/platform/ocp/1
[ 12.100176] remoteproc1: Note: remoteproc is still under development and considered experimental.
[ 12.194559] remoteproc1: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 12.359795] remoteproc1: registered virtio0 (type 7)
[ 12.364982] pru-rproc 4a334000.pru0: PRU rproc node /ocp/pruss@4a300000/pru0@4a334000 probed successfully
[ 12.469497] remoteproc2: 4a338000.pru1 is available
[ 12.474521] remoteproc2: Note: remoteproc is still under development and considered experimental.
[ 12.690845] remoteproc2: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 12.832472] remoteproc2: registered virtio1 (type 7)
[ 12.848934] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ 12.883021] pru-rproc 4a338000.pru1: PRU rproc node /ocp/pruss@4a300000/pru1@4a338000 probed successfully
[ 12.970296] systemd[1]: Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.
[ OK ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.
[ 13.780609] systemd[1]: Found device /dev/mmcblk0p1.
[ OK ] Found device /dev/mmcblk0p1.
[ 15.989852] usbcore: registered new interface driver usbfs
[ 15.995475] usbcore: registered new interface driver hub
[ 16.060144] usbcore: registered new device driver usb
[ 16.198436] musb-hdrc musb-hdrc.0.auto: MUSB HDRC host driver
[ 16.204255] musb-hdrc musb-hdrc.0.auto: new USB bus registered, assigned bus number 1
[ 16.335308] hub 1-0:1.0: USB hub found
[ 16.375938] hub 1-0:1.0: 1 port detected
[ 16.424450] musb-hdrc musb-hdrc.1.auto: MUSB HDRC host driver
[ 16.446032] remoteproc1: powering up 4a334000.pru0
[ 16.451486] remoteproc1: Booting fw image am335x-pru0-fw, size 75576
[ 16.508334] musb-hdrc musb-hdrc.1.auto: new USB bus registered, assigned bus number 2
[ 16.526012] ti-pruss 4a300000.pruss: configured system_events = 0x0000000000030000 intr_channels = 0x00000005 host_intr = 0x00000005
[ 16.548959] hub 2-0:1.0: USB hub found
[ 16.576074] hub 2-0:1.0: 1 port detected
[ 16.580371] remoteproc1: remote processor 4a334000.pru0 is now up
[ 16.587653] virtio_rpmsg_bus virtio0: creating channel rpmsg-pru addr 0x1e
[ 16.595395] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 16.636425] remoteproc2: powering up 4a338000.pru1
[ 16.641931] remoteproc2: Booting fw image am335x-pru1-fw, size 75576
[ 16.701396] ti-pruss 4a300000.pruss: configured system_events = 0x00000000000c0000 intr_channels = 0x0000000a host_intr = 0x0000000a
[ 16.785999] remoteproc2: remote processor 4a338000.pru1 is now up
[ 16.792551] virtio_rpmsg_bus virtio1: creating channel rpmsg-pru addr 0x1f
[ 16.815763] virtio_rpmsg_bus virtio1: rpmsg host is online
[ 16.922617] rpmsg_pru rpmsg0: new rpmsg_pru device: /dev/rpmsg_pru30
[ 16.957792] rpmsg_pru rpmsg1: new rpmsg_pru device: /dev/rpmsg_pru31
[ 17.196780] musb-hdrc musb-hdrc.1.auto: VBUS_ERROR in a_wait_vrise (80, <SessEnd), retry #3, port1 0008010c
[ *** ] (2 of 4) A start job is running for dev-ttyO3.device (16s / 1min 30s)
This happens both on the EVMSK and on our board so it's not a HW problem.
BTW, these "jobs" follow one another and never end. Any suggestions?