This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/BEAGLEBK: Sitara Audio DAC Example update for Processor SDK

Part Number: BEAGLEBK

Tool/software: Linux

Hi, Texas Team!

Sitara Audio DAC Example (processors.wiki.ti.com/.../Sitara_Linux_Audio_DAC_Example) with SDK 7.0 (Kernel 3.12) is a great help in audio driver development!

Wiht the new Processor SDK and Linux Kernel 4.4, things changed  a lot and some steps in the audio dac example are not valid anymore (for instance: "Use an existing structure as a template: snd_soc_dai_link evm_dai_tda998x_hdmi will work well for this. It is located around line 630.").

Is it possible to update it! It would be much appreciated!

Best Regards!