This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM365 - DVSDK 1080p encode issue



Hi all

I want to know that encode 1080p in dm365. (MPEG2 or MPEG4 codec)

So, i tred to encode 1080p in dvsdk_2_10_01_18. (dvsdk_3_10_00_16 also...)

But resolutions are encoding  error... 

Does dvsdk support up to 720p?

If so, how to setup dvsdk for encode 1080p.

Thanks.

* My dvsdk version : dvsdk_2_10_01_18 or dvsdk_3_10_00_16

   Encode Codec : MPEG2 or MPEG4

  • Hi,

    Can you confirm the version of MPEG4 and MPEG2 codec that you are using? The support for 1080P resolution exist for the codecs, but i can confirm based on the version number. Meanwhile, are you able to capture a 1080P resolution data or do you want to have a file based encode application where 1080P input is read from the file? Inherently, DVSDK does not have support for 1080P resolution capture and changes would have to be done inthe demos for the same.

    Regards,

    Anshuman