Other Parts Discussed in Thread: TPS51200
pg 17 of
DDR3 Design Requirements for KeyStone Devices read as follows:
Limitations on DC voltage tolerance and AC noise for all reference voltages is well
defined in the applicable JEDEC standard (pg. 129 of JESD79-3C). Strict conformity to
these limitations is important to help ensure proper functionality of the DDR3 SDRAM
interface. The Vref tolerance is ・}1% or VDD/2 ・}1%, which equates to
0.7425 V – 0.7575 V. To achieve this tight tolerance, it is recommended (when using a
standard resistor divider network) that better than 1% tolerance components be used.
But upon looking at the data sheet
SPRS814C –MARCH 2012–REVISED MAY 2016
pg 36 for the device it reads:
VREFSSTL DDR3 reference voltage 0.49 × DVDD15 0.5 × DVDD15 0.51 × DVDD15 V
The data sheet gives more relaxinf requiremetns!
I think I read somewhere that the data sheet overules the other documents.....Im using the TPS51200 termination supply which gives the tolerance for refout as 0.75 V plus or minus 15 mV which meets the data sheet requirements but not the other document requirements....
Is the TPS51200 ok to use?