This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/OMAP4460: error setting wl12xx data: -38

Part Number: OMAP4460


Tool/software: Linux

Hi friends, I am trying to boot 'Panda board ES rev B1 ( OMAP4460 )' . I download the pre-built image "ubuntu-12.04-preinstalled-desktop-armhf+omap4.img.gz" and port it into the SD card. I got the command prompt, but my board reboot itself after few seconds and when i connect ethernet or any USB device, it reboot itself simultaneously and before comming command prompt it reboot itself again n again. After some researches, but i din't get any perfect solution. So thinking as a driver issue, i download '3.4.113 kernel' from the kernel.org, cross compile for pandaboard with default configuration file i.e 'omap2plus_defconfig' . Now my board is booting perfectly, but there is no ethernet and usb driver found, and also WLAN failng. when i enter command 'ifconfig' , it prints only loopback address. I need to enable WLAN, ethernet and usb driver, but not getting any perfect solution. Can anyone please help me... Thanks & Regards Ravi