Hello,
There are multiple reserved pins in the K2E SoC. These pins are connected to test points.
I noted that, there are three types of test points used for reserved pins. Also some reserved pins are directly connected to test point and some are through 0E Res.
Why these test points are provided on reserved pins and why there is a mismatch between test point type and why some have 0E res and some do not have.
According to K2E SoC, these reserved pins should be NC, can we left these pins NC?
Thanks and Regards
Tarang Jindal