Part Number: TMS320C6748
Other Parts Discussed in Thread: TSC2007
Tool/software: Starterware
Hi TI Experts:
I use LCDK6748 to interface with TSC 2007 chip, I used starterWare-1-20-04-01 I2C interface program codecif.c to talk to TSC2007. I2C interface program works well in Main program, I can read/write data from TSC2007. when I move the I2C program to ISR routine, It stops. I use GPOI2-6 fall edge to trigger ISR. It enters to ISR, then stuck to I2C. What do I missed when I use I2C read/write in ISR? I used mask_INT4 for I2C, and mask_INT6 for GPIO interrupt. In the GPIO interrupt ISR, I2C read/write is included.