Other Parts Discussed in Thread: OMAP-L137, SYSBIOS
Hello,
I've a question related to the rta agent for the ARM on the OMAP-L137.
On the ARM side of the OMAP the following version are used:
- BIOS Version: bios_6_20_01_41
- CCS Version : 4.0.1.01001
When adding the ti.sysbios.rta.Agent to my configuration and build the project,
I got the error, that "RTA Agent not supported on Arm targets.":
Turning on task names...
error: ti.sysbios.rta.Agent: "C:/Program Files/Texas Instruments/bios_6_20_01_41/packages/ti/sysbios/rta/Agent.xs", line 59: ti.sysbios.rta.Agent : RTA Agent not supported on Arm targets.
js: "C:/Program Files/Texas Instruments/xdctools_3_15_02_62/packages/xdc/cfg/Main.xs", line 115: Error: Configuration failed!
In the meantime newer BIOS and CCS version are available.
With which BIOS/CCS versions is RTA for the ARM (as part of the OMAP-L137) supported?
Thanks,
Frank