Hi
I'm trying to download a 640x480 frame from an aptina CMOS sensor using ISIF directy to the SDRAM base address.
I try dirctly from uboot. and I configure the ISIF inferface with this script
-----------------------------------------------
mw.l 01C71004 0000 1
mw.l 01C71018 0000 1
mw.l 01C7101c 01e0 1
mw.l 01C71020 0000 1
mw.l 01C71024 0000 1
mw.l 01C71028 0280 1
mw.l 01C71034 0028 1
mw.l 01C71038 0000 1
mw.l 01C7103c 0000 1
mw.l 01C71040 0000 1
mw.l 01C71070 0010 1
mw.l 01C71074 0200 1
mw.l 01C71078 0300 1
mw.l 01C71000 0003 1
----------------------------------------
IPIPE_IF and ISIF interrupt comes. But no data is found at 0x80000000
can we help me?