Tool/software: TI-RTOS
Hi,
I’m an typical EE coming from the digital world hitting the RTOS ceiling.
We are using the 66AK2G02 device.
May I ask you, if you recommend using TI-RTOS for the following application:
We want to control a 60-phase E-motor (which we actually implement in an automobile to drive around with :-). We have a rather complex Simulink model which we would like to compile on the C66X. The A15 should do the control of the system, CAN Bus handling, Fuzzy logic, and the “inner loop timing” of the MotorControl Circuit. We hope to achieve a Control Frequency of 100kHz. PWM generation and Current ADC readout are done outside the K2G device.
Most importantly, we need the Ethernet interface (simple UDP would be enough) for motor control data monitoring.
May I use this excellent forum for this simple question:
Can we guarantee with TI-RTOS an exact 100kHz output pulse while organizing the rest of the payload. Do we have to use TI-RTOS when we want to reuse an UDP EMAC driver. Would you rather do this with bare metal code 66AK2G02 ?
A recommendation is highly appreciated,
thank you in advance,
Best Regards, Tobias