Other Parts Discussed in Thread: OMAP3525, OMAP3530, OMAP3503, TLK6002
Hello,
I have a question, is it OMAP3530, OMAP3525 and OMAP3503 capture symbols the same symbol? I only can find the first one.
Thanks,
Fernando.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Fernando Carrio said:I have a question, is it OMAP3530, OMAP3525 and OMAP3503 capture symbols the same symbol?
Yes, the OMAP3530 schematic symbol should be suitable for OMAP3525 or OMAP3503 as well, as they share the same physical packages and pin outs, the symbol just happens to be labeled with the super set device's part number (other OMAP35xx devices are the same device just missing either the SGX graphics accelerator, the C64x+ DSP, or both).
Ok, thanks. What about TLK6002? I cannot find any symbol & footprint? there is any similar?
Thanks,
Fernando.