This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5718: Which pad to use for PMIC_INT

Part Number: AM5718
Other Parts Discussed in Thread: AM5728, , TPS22965

Hello, 

In the AM5728 ref design , the WAKEUP0 pad is used for the PMIC_INT signal on the TPS22965. However, on the AM5718 RDK the GPIO6_16 pad is used for PMIC_INT which does not have a wakeup muxing option. According to the latest AM571x/AM572x compatibility document the WAKEUP0 pad on the AM5718 supports a wakeup muxing option and a gpio option but the wording is not clear. Our design is required to  to support both processors depending on the BOM option, and I wanted to see if using the WAKEUP0 pin on the AM5718 as the PMIC_INT will cause any issues.

Cheers

S.V