This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/DRA718: IEEE 1588 on JACINTO J6 DRAXX

Part Number: DRA718

Tool/software: Linux

Hi Team:

               We have a Ethernet AVB stack of our own. We are looking for TI Evaluation Bords / SOCs which can be used to port and test the AVB stack code. 

Questions:

For the JACINTO 6 EVM ( DRAXX Jacinto Faimly ) :

1. Does MAC ports have hardware support for IEEE1588 .

2. Does the hardware also support for queue managment ( Rx/Tx ) and traffic Shapping  ( Tx only ) ?

3. Will the TI OS provide the 1588 PTP support to Map and use the PTP functionality. 

If this is not there on Jacinto which other board/SOC will provide this support? 

Regards,

Amit Mehra