Part Number: AM3359
Tool/software: Linux
Hello there,
I have been able to setup a CAN bus ( with CAN0 and CAN1) by making one sending and the other receiving without problems.
./ip link set can0 up type can bitrate 125000 listen-only on loopback off restart-ms 100
./ip link set can1 up type can bitrate 125000 listen-only off loopback on restart-ms 100
./cangen can1 -e
./candump can0
with ifconfig i can also see that the received and transmited packets increment. Bellow you see my output.
root@TQMa335x:~/can-bus ./ip -det -stat link show can0
2: can0: <NOARP,UP,LOWER_UP,ECHO> mtu 16 qdisc pfifo_fast state UNKNOWN qlen 10
link/can
can <LISTEN-ONLY> state ERROR-ACTIVE (berr-counter tx 0 rx 0) restart-ms 100
bitrate 125000 sample-point 0.875
tq 500 prop-seg 6 phase-seg1 7 phase-seg2 2 sjw 1
c_can: tseg1 2..16 tseg2 1..8 sjw 1..4 brp 1..1024 brp-inc 1
clock 26000000
re-started bus-errors arbit-lost error-warn error-pass bus-off
0 0 0 3 3 0
RX: bytes packets errors dropped overrun mcast
138353 23929 0 0 0 0
TX: bytes packets errors dropped carrier collsns
104340 18060 0 16 0 0
root@TQMa335x:~/can-bus ./ip -det -stat link show can1
3: can1: <NOARP,UP,LOWER_UP,ECHO> mtu 16 qdisc pfifo_fast state UP qlen 10
link/can
can <LOOPBACK> state ERROR-ACTIVE (berr-counter tx 0 rx 0) restart-ms 100
bitrate 125000 sample-point 0.875
tq 500 prop-seg 6 phase-seg1 7 phase-seg2 2 sjw 1
c_can: tseg1 2..16 tseg2 1..8 sjw 1..4 brp 1..1024 brp-inc 1
clock 26000000
re-started bus-errors arbit-lost error-warn error-pass bus-off
0 0 0 1 2 1
RX: bytes packets errors dropped overrun mcast
555424 75849 1 0 1 0
TX: bytes packets errors dropped carrier collsns
35943 6196 0 32 0 0
->Now the problem comes up when I connect my CAN0 to a separate bus (Extended CAN). I only want to monitor the traffic on the bus.
After i connect it the ERROR-ACTIVE changes to ERROR-PASSIVE and I am not able to see anything from the bus. ifconfig doenst shows any sign of communication going on neither.
root@TQMa335x:~/can-bus ./ip -det -stat link show can0
2: can0: <NOARP,UP,LOWER_UP,ECHO> mtu 16 qdisc pfifo_fast state UNKNOWN qlen 10
link/can
can <LISTEN-ONLY> state ERROR-PASSIVE (berr-counter tx 0 rx 127) restart-ms 100
bitrate 125000 sample-point 0.875
tq 500 prop-seg 6 phase-seg1 7 phase-seg2 2 sjw 1
c_can: tseg1 2..16 tseg2 1..8 sjw 1..4 brp 1..1024 brp-inc 1
clock 26000000
re-started bus-errors arbit-lost error-warn error-pass bus-off
0 0 0 4 4 0
RX: bytes packets errors dropped overrun mcast
148920 25756 0 0 0 0
TX: bytes packets errors dropped carrier collsns
104340 18060 0 16 0 0
The only reason that can happen is that my separate bus is transmitting errors that my CAN0 node detects and increments in the counter.
But why am I not able to see the errors or the frames being transmitted ?
Or how can I setup to ignore the errors and sniff on the bus?
Much appreciated for any help.
Greetings,
Pedro