Part Number: 66AK2L06
I have a custom board designed around the 66AK2L06.
I'm using CCS v7 with an XDS100v3.
Power-up/Clocking/Reset sequence appears to be OK since I have RESET STATUS going high and a 16.666mHz clock on the SYSCLKOUT pin.
CVDD is controlling around 0.94v
Running the JTAG 'Test Connnection' has no errors.
Bootmode pins set to Sleep Mode with ARM boot and PLL/System clock set to 1Ghz (100mHz input clock).
The problem is when I try to run a short test program in debug. The GEL loads and executes but I get the following error:
ARM_A15_0: Trouble Halting CPU (Error -1321). Device failed to enter debug/halt mode because security settings prevent debug.
I'm not sure what security settings they are talking about. Any ides on what I can try to debug/fix this?
Thanks!