Other Parts Discussed in Thread: AM5718, DRA722, PMP, TLC59108, DRA72, AM5728, DRA742
Tool/software: Linux
Hi,
We developed a new custom board with AM5718 processor and using ti-processor-sdk-linux-am57xx-evm-02.00.01.07. When I am trying to boot the board withSD card, the kernel hangs at starting kernel sometimes and sometimes booting up to some point , please check the log when it not hangs at starting kernel,
U-Boot SPL 2015.07-00080-g4523775-dirty (Jan 28 2017 - 17:27:57)
DRA722 ES1.0
console init >>sdram_init()
in_sdram = 0
>>do_sdram_init() 4c000000
CONFIG_SYS_EMIF_PRECALCULATED_TIMING_REGSHW leveling success
<<do_sdram_init() 4c000000
max size is 40000000get_ram_size() successful<<sdram_init()
>>spl:board_init_r()
using memory 0x80a80000-0x81a80000 for malloc()
spl board init start
U-Boot SPL 2015.07-00080-g4523775-dirty (Jan 28 2017 - 17:27:57)
DRA722 ES1.0
spl board init boot device - 5
CONFIG_SPL_MMC_SUPPORT = 5
Entered spl_mmc_load_image 1076960188
Entered board_mmc_init
Entered omap_mmc_init
Size required 44
Sufficient Memory for priv_data
OMAP_HSMMC1_BASE
mmc1 device created
Entered do_preinit
List Entry
m->preinit = 0
List Exit
No mmc_start_init
Exit do_preinit
Searching mmc device mmc - -2136473544
mmc_init: 0, time 65
err - 0
boot_mode - 2 1
spl: mmc boot mode: fs
reading args
VFAT Support enabled
FAT read(sect=2256, cnt:1), clust_size=1, DIRENTSPERBLOCK=16
RootMismatch: |mlo||
Rootvfatname: |u-boot.img|
RootMismatch: |u-boot.img|u-boot.img|
RootMismatch: |u-boot.img||
Rootvfatname: |uenv.txt|
RootMismatch: |uenv.txt|uenv.txt|
RootMismatch: |uenv.txt||
RootDentname == NULL - 6
spl_load_image_fat_os: error reading image args, err - -1
reading u-boot.img
VFAT Support enabled
FAT read(sect=2256, cnt:1), clust_size=1, DIRENTSPERBLOCK=16
RootMismatch: |mlo||
Rootvfatname: |u-boot.img|
RootName: u-boot.img, start: 0x9e9, size: 0x5e348
Filesize: 385864 bytes
64 bytes
gc - clustnum: 2537, startsect: 4791
Size: 385864, got: 64
spl: payload image: U-Bo load addr: 0x807fffc0 size: 385864
reading u-boot.img
VFAT Support enabled
FAT read(sect=2256, cnt:1), clust_size=1, DIRENTSPERBLOCK=16
RootMismatch: |mlo||
Rootvfatname: |u-boot.img|
RootName: u-boot.img, start: 0x9e9, size: 0x5e348
Filesize: 385864 bytes
385864 bytes
gc - clustnum: 2537, startsect: 4791
Size: 385864, got: 385864
Jumping to U-Boot
image entry point: 0x80800000
i2c_probe: pads on bus 0 probably not configured (status=0x10)
ti_i2c_eeprom_init failed 1
initcall: 8082fda9
U-Boot 2015.07-00080-g4523775-dirty (Jan 28 2017 - 17:27:57 +0530)
initcall: 8080471d
U-Boot code: 80800000 -> 80853128 BSS: -> 808A2534
initcall: 808008f1
CPU : DRA722 ES1.0
initcall: 80804a65
Board: UNKNOWN(BeagleBoard X15?)
initcall: 80804751
I2C: ready
initcall: 80804741
DRAM: initcall: 808008c9
>>sdram_init()
initcall: 80804879
Monitor len: 000A2534
Ram size: 40000000
Ram top: C0000000
initcall: 80804551
initcall: 808046d5
TLB table from bfff0000 to bfff4000
initcall: 80804565
initcall: 80804695
Reserving 649k for U-Boot at: bff4d000
initcall: 8080466d
Reserving 16448k for malloc() at: bef3d000
initcall: 80804799
Reserving 88 Bytes for Board Info at: bef3cfa8
initcall: 80804569
initcall: 80804645
Reserving 184 Bytes for Global Data at: bef3cef0
initcall: 808045f5
initcall: 80804571
initcall: 808048d5
initcall: 8080485d
initcall: 808047d9
RAM Configuration:
Bank #0: 80000000 Bank #1: 0
DRAM: 1 GiB
initcall: 808045e1
New Stack Pointer is: bef3ced0
initcall: 80804579
initcall: 8080459d
Relocation Offset is: 3f74d000
Relocating to bff4d000, new gd at bef3cef0, sp at bef3ced0
initcall: bff51915
initcall: bff51a2b
initcall: 80804a21 (relocated to bff51a21)
dram_bank_mmu_setup: bank: 0
dram_bank_mmu_setup: bank: 1
initcall: 80804919 (relocated to bff51919)
initcall: 80804935 (relocated to bff51935)
initcall: 80804a05 (relocated to bff51a05)
using memory 0xbef3d000-0xbff4d000 for malloc()
initcall: 80804911 (relocated to bff51911)
initcall: 808029e1 (relocated to bff4f9e1)
initcall: 808142c1 (relocated to bff612c1)
initcall: 808049f9 (relocated to bff519f9)
initcall: 808049e5 (relocated to bff519e5)
Now running in RAM - U-Boot at: bff4d000
initcall: 80804939 (relocated to bff51939)
initcall: 808049d1 (relocated to bff519d1)
NAND:
Initalising NAND Memorynand: selected OMAP_ECC_BCH8_CODE_HW
Scanning NAND Memory0 MiB
initcall: 808049b9 (relocated to bff519b9)
MMC:
Entered omap_mmc_init
Size required 44
Sufficient Memory for priv_data
OMAP_HSMMC1_BASE
mmc1 device created
Entered omap_mmc_init
Size required 44
Sufficient Memory for priv_data
mmc1 device created OMAP SD/MMC: 0, OMAP SD/MMC: 1
Entered do_preinit
List Entry
m->preinit = 0
List Exit
No mmc_start_init
List Entry
m->preinit = 0
List Exit
No mmc_start_init
Exit do_preinitinitcall: 80804999 (relocated to bff51999)
mmc_init: 0, time 65
reading uboot.env
VFAT Support enabled
FAT read(sect=2256, cnt:1), clust_size=1, DIRENTSPERBLOCK=16
RootMismatch: |mlo||
Rootvfatname: |u-boot.img|
RootMismatch: |u-boot.img|u-boot.img|
RootMismatch: |u-boot.img||
Rootvfatname: |uenv.txt|
RootMismatch: |uenv.txt|uenv.txt|
RootMismatch: |uenv.txt||
RootDentname == NULL - 6
** Unable to read "uboot.env" from mmc0:1 **
Using default environment
Destroy Hash Table: bff9b6e0 table = 00000000
Create Hash Table: N=512
INSERT: table bff9b6e0, filled 1/521 rv bef3f4a4 ==> name="bootcmd" value="if test ${dofastboot} -eq 1; then echo Boot fastboot requested, res"
INSERT: table bff9b6e0, filled 2/521 rv bef3fd00 ==> name="bootdelay" value="1"
INSERT: table bff9b6e0, filled 3/521 rv bef3f080 ==> name="baudrate" value="115200"
INSERT: table bff9b6e0, filled 4/521 rv bef3e89c ==> name="arch" value="arm"
INSERT: table bff9b6e0, filled 5/521 rv bef40098 ==> name="cpu" value="armv7"
INSERT: table bff9b6e0, filled 6/521 rv bef3f850 ==> name="board" value="am57xx"
INSERT: table bff9b6e0, filled 7/521 rv bef3eb58 ==> name="board_name" value="am57xx"
INSERT: table bff9b6e0, filled 8/521 rv bef40124 ==> name="vendor" value="ti"
INSERT: table bff9b6e0, filled 9/521 rv bef406ec ==> name="soc" value="omap5"
INSERT: table bff9b6e0, filled 10/521 rv bef3fb84 ==> name="loadaddr" value="0x82000000"
INSERT: table bff9b6e0, filled 11/521 rv bef3f508 ==> name="kernel_addr_r" value="0x82000000"
INSERT: table bff9b6e0, filled 12/521 rv bef3fea4 ==> name="fdtaddr" value="0x88000000"
INSERT: table bff9b6e0, filled 13/521 rv bef3ee64 ==> name="fdt_addr_r" value="0x88000000"
INSERT: table bff9b6e0, filled 14/521 rv bef3fcec ==> name="rdaddr" value="0x88080000"
INSERT: table bff9b6e0, filled 15/521 rv bef40228 ==> name="ramdisk_addr_r" value="0x88080000"
INSERT: table bff9b6e0, filled 16/521 rv bef3e4dc ==> name="bootm_size" value="0x10000000"
INSERT: table bff9b6e0, filled 17/521 rv bef3e9a0 ==> name="mmcdev" value="0"
INSERT: table bff9b6e0, filled 18/521 rv bef3f6ac ==> name="mmcrootfstype" value="ext4 rootwait"
INSERT: table bff9b6e0, filled 19/521 rv bef3ef18 ==> name="finduuid" value="part uuid mmc 0:2 uuid"
INSERT: table bff9b6e0, filled 20/521 rv bef3f008 ==> name="args_mmc" value="run finduuid;setenv bootargs console=${console} ${optargs} root=P"
INSERT: table bff9b6e0, filled 21/521 rv bef3e680 ==> name="loadbootscript" value="load mmc ${mmcdev} ${loadaddr} boot.scr"
INSERT: table bff9b6e0, filled 22/521 rv bef3efe0 ==> name="bootscript" value="echo Running bootscript from mmc${mmcdev} ...; source ${loadadd"
INSERT: table bff9b6e0, filled 23/521 rv bef3f8b4 ==> name="bootenvfile" value="uEnv.txt"
INSERT: table bff9b6e0, filled 24/521 rv bef3ecd4 ==> name="importbootenv" value="echo Importing environment from mmc${mmcdev} ...; env import"
INSERT: table bff9b6e0, filled 25/521 rv bef40c8c ==> name="loadbootenv" value="fatload mmc ${mmcdev} ${loadaddr} ${bootenvfile}"
INSERT: table bff9b6e0, filled 26/521 rv bef3ed10 ==> name="envboot" value="mmc dev ${mmcdev}; if mmc rescan; then echo SD/MMC found on device"
INSERT: table bff9b6e0, filled 27/521 rv bef406b0 ==> name="console" value="ttyO0,115200n8 root=PARTUUID=00000000-02 rw mem=512M rootfstype=ex"
INSERT: table bff9b6e0, filled 28/521 rv bef3f9a4 ==> name="fdtfile" value="undefined"
INSERT: table bff9b6e0, filled 29/521 rv bef40890 ==> name="bootpart" value="0:2"
INSERT: table bff9b6e0, filled 30/521 rv bef3e478 ==> name="bootdir" value="/boot"
INSERT: table bff9b6e0, filled 31/521 rv bef3f7c4 ==> name="bootfile" value="zImage"
INSERT: table bff9b6e0, filled 32/521 rv bef3f198 ==> name="usbtty" value="cdc_acm"
INSERT: table bff9b6e0, filled 33/521 rv bef3f788 ==> name="vram" value="16M"
INSERT: table bff9b6e0, filled 34/521 rv bef400ac ==> name="partitions" value="uuid_disk=${uuid_gpt_disk};name=rootfs,start=2MiB,size=-,uuid=$"
DELETE CANDIDATE: "optargs"
hdelete: DELETE key "optargs"
DELETE ERROR ##############################
INSERT: table bff9b6e0, filled 35/521 rv bef3e734 ==> name="dofastboot" value="0"
INSERT: table bff9b6e0, filled 35/521 rv bef3e680 ==> name="loadbootscript" value="fatload mmc ${mmcdev} ${loadaddr} boot.scr"
INSERT: table bff9b6e0, filled 35/521 rv bef3efe0 ==> name="bootscript" value="echo Running bootscript from mmc${mmcdev} ...; source ${loadadd"
INSERT: table bff9b6e0, filled 36/521 rv bef3fe2c ==> name="loadimage" value="load mmc ${bootpart} ${loadaddr} ${bootdir}/${bootfile}"
INSERT: table bff9b6e0, filled 37/521 rv bef40778 ==> name="mmcboot" value="mmc dev ${mmcdev}; if mmc rescan; then echo SD/MMC found on device"
INSERT: table bff9b6e0, filled 38/521 rv bef40994 ==> name="findfdt" value="if test $board_name = omap5_uevm; then setenv fdtfile omap5-uevm.d"
INSERT: table bff9b6e0, filled 39/521 rv bef401c4 ==> name="loadfdt" value="load mmc ${bootpart} ${fdtaddr} ${bootdir}/${fdtfile};"
INSERT: table bff9b6e0, filled 40/521 rv bef3eedc ==> name="dfu_bufsiz" value="0x10000"
INSERT: table bff9b6e0, filled 41/521 rv bef3f350 ==> name="dfu_alt_info_mmc" value="boot part 0 1;rootfs part 0 2;MLO fat 0 1;MLO.raw raw 0x1"
INSERT: table bff9b6e0, filled 42/521 rv bef3fd14 ==> name="dfu_alt_info_emmc" value="rawemmc raw 0 3751936;boot part 1 1;rootfs part 1 2;MLO "
INSERT: table bff9b6e0, filled 43/521 rv bef3ed9c ==> name="dfu_alt_info_ram" value="kernel ram 0x80200000 0x4000000;fdt ram 0x80f80000 0x8000"
INSERT: table bff9b6e0, filled 44/521 rv bef406d8 ==> name="dfu_alt_info_qspi" value="MLO raw 0x0 0x010000;MLO.backup1 raw 0x010000 0x010000;M"
INSERT: table bff9b6e0, filled 45/521 rv bef407f0 ==> name="static_ip" value="${ipaddr}:${serverip}:${gatewayip}:${netmask}:${hostname}::off"
INSERT: table bff9b6e0, filled 46/521 rv bef3ff58 ==> name="nfsopts" value="nolock"
INSERT: table bff9b6e0, filled 47/521 rv bef3fddc ==> name="rootpath" value="/export/rootfs"
INSERT: table bff9b6e0, filled 48/521 rv bef3e7d4 ==> name="netloadimage" value="tftp ${loadaddr} ${bootfile}"
INSERT: table bff9b6e0, filled 49/521 rv bef3f7ec ==> name="netloadfdt" value="tftp ${fdtaddr} ${fdtfile}"
INSERT: table bff9b6e0, filled 50/521 rv bef3fad0 ==> name="netargs" value="setenv bootargs console=${console} ${optargs} root=/dev/nfs nfsroo"
INSERT: table bff9b6e0, filled 51/521 rv bef40bec ==> name="netboot" value="echo Booting from network ...; setenv autoload no; dhcp; run netlo"
INSERT: free(data = bef3d308)
INSERT: done
initcall: 80804a49 (relocated to bff51a49)
initcall: 808142d5 (relocated to bff612d5)
initcall: 8080498f (relocated to bff5198f)
initcall: 80812b79 (relocated to bff5fb79)
Initial value for argc=3
Final value for argc=3
Initial value for argc=3
Final value for argc=3
Initial value for argc=3
Final value for argc=3
initcall: 808025dd (relocated to bff4f5dd)
initcall: 80804985 (relocated to bff51985)
initcall: 8080496d (relocated to bff5196d)
initcall: 808029f9 (relocated to bff4f9f9)
i2c_probe: pads on bus 0 probably not configured (status=0x10)
Invalid EEPROM data(@0x4031e028). Default to X15
Initial value for argc=3
Final value for argc=3
Initial value for argc=2
Final value for argc=2
hdelete: DELETE key "board_rev"
Initial value for argc=2
Final value for argc=2
hdelete: DELETE key "board_serial"
i2c_write: pads on bus 0 probably not configured (status=0x10)
initcall: 80804959 (relocated to bff51959)
SCSI: ahci_host_init: start
cap 0xef26ff80 port_map 0x1 n_ports 1
SATA link 0 timeout.
HOST_CTL 0x80000000
HOST_CTL 0x80000002
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Enter ahci_device_data_io: for port 0
No Link on port 0!
scsi_ahci: SCSI inquiry command failure.
SCSI command 0x12 ret errno -5
Found 0 device(s).
Initial value for argc=3
Final value for argc=3
initcall: 80804945 (relocated to bff51945)
Net: <ethaddr> not set. Validating first E-fuse MAC
Initial value for argc=3
Final value for argc=3
Initial value for argc=3
Final value for argc=3
Initial value for argc=3
Final value for argc=3
Phy 1 not found
PHY status read failed
cpsw connected to Generic PHY
cpsw
initcall: 8080493d (relocated to bff5193d)
Initial value for argc=3
Final value for argc=3
### main_loop entered: bootdelay=1
### main_loop: bootcmd="if test ${dofastboot} -eq 1; then echo Boot fastboot requested, resetting dofastboot ...;setenv dofastboot 0; saveenv;"
Hit any key to stop autoboot: 0
: returns 1
Command failed, result=1: returns 1
Command failed, result=1: returns 1
Command failed, result=1: returns 1
Command failed, result=1: returns 0
Initial value for argc=3
Final value for argc=3
: returns 1
Command failed, result=1: returns 1
Command failed, result=1: returns 1
Command failed, result=1: returns 1
Command failed, result=1: returns 1
Command failed, result=1: returns 1
Command failed, result=1Command failed, result=1mmc_init: 0, time 66
switch to partitions #0, OK
mmc0 is current device
mmc_init: 0, time 65
SD/MMC found on device 0
reading boot.scr
VFAT Support enabled
FAT read(sect=2256, cnt:1), clust_size=1, DIRENTSPERBLOCK=16
RootMismatch: |mlo||
Rootvfatname: |u-boot.img|
RootMismatch: |u-boot.img|u-boot.img|
RootMismatch: |u-boot.img||
Rootvfatname: |uenv.txt|
RootMismatch: |uenv.txt|uenv.txt|
RootMismatch: |uenv.txt||
RootDentname == NULL - 6
** Unable to read file boot.scr **
Command failed, result=1Command failed, result=1reading uEnv.txt
VFAT Support enabled
FAT read(sect=2256, cnt:1), clust_size=1, DIRENTSPERBLOCK=16
RootMismatch: |mlo||
Rootvfatname: |u-boot.img|
RootMismatch: |u-boot.img|u-boot.img|
RootMismatch: |u-boot.img||
Rootvfatname: |uenv.txt|
RootName: uenv.txt, start: 0x2ac, size: 0x23e
Filesize: 574 bytes
574 bytes
gc - clustnum: 684, startsect: 2938
Size: 574, got: 574
574 bytes read in 37 ms (14.6 KiB/s)
Initial value for argc=3
Final value for argc=3
Loaded env from uEnv.txt
Importing environment from mmc0 ...
INSERT: free(data = bef436e0)
INSERT: done
Command failed, result=1Command failed, result=1mmc_init: 0, time 66
switch to partitions #0, OK
mmc0 is current device
mmc_init: 0, time 65
SD/MMC found on device 0
<2, 0, 1024>
EXT2 rev 1, inode_size 256
ext4fs read 0 group descriptor (blkno 1 blkoff 0)
<8, 0, 32>
<1848, 256, 128>
<5872, 0, 8>
<5872, 8, 1>
<5872, 12, 8>
<5872, 20, 2>
<5872, 24, 8>
<5872, 32, 3>
<5872, 36, 8>
<5872, 44, 3>
<5872, 48, 8>
<5872, 56, 3>
<5872, 60, 8>
<5872, 68, 3>
<5872, 72, 8>
<5872, 80, 3>
<5872, 84, 8>
<5872, 92, 3>
<5872, 96, 8>
<5872, 104, 4>
<5872, 108, 8>
<5872, 116, 4>
ext4fs read 15 group descriptor (blkno 1 blkoff 480)
<8, 480, 32>
<3932176, 0, 128>
<3936200, 0, 8>
<3936200, 8, 1>
<3936200, 12, 8>
<3936200, 20, 2>
<3936200, 24, 8>
<3936200, 32, 40>
<3936200, 72, 8>
<3936200, 80, 40>
<3936200, 120, 8>
<3936200, 128, 6>
ext4fs read 15 group descriptor (blkno 1 blkoff 480)
<8, 480, 32>
<3932177, 256, 128>
Got symlink >zImage-4.1.13-g8dc6617<
ext4fs read 15 group descriptor (blkno 1 blkoff 480)
<8, 480, 32>
<3932176, 0, 128>
<3936200, 0, 8>
<3936200, 8, 1>
<3936200, 12, 8>
<3936200, 20, 2>
<3936200, 24, 8>
<3936200, 32, 40>
<3936200, 72, 8>
<3936200, 80, 40>
<3936200, 120, 8>
<3936200, 128, 6>
<3936200, 136, 8>
<3936200, 144, 23>
<3936200, 168, 8>
<3936200, 176, 21>
<3936200, 200, 8>
<3936200, 208, 22>
ext4fs read 15 group descriptor (blkno 1 blkoff 480)
<8, 480, 32>
<3932179, 0, 128>
<3942552, 0, 4096>
<4046848, 0, 65536>
<200576, 0, 65536>
<201216, 0, 131072>
<203008, 0, 262144>
<203776, 0, 524288>
<222208, 0, 1048576>
<225280, 0, 1248280>
3345432 bytes read in 320 ms (10 MiB/s)
Initial value for argc=3
Final value for argc=3
<2, 0, 1024>
EXT2 rev 1, inode_size 256
ext4fs read 0 group descriptor (blkno 1 blkoff 0)
<8, 0, 32>
<1848, 256, 128>
<5872, 0, 8>
<5872, 8, 1>
<5872, 12, 8>
<5872, 20, 2>
<5872, 24, 8>
<5872, 32, 3>
<5872, 36, 8>
<5872, 44, 3>
<5872, 48, 8>
<5872, 56, 3>
<5872, 60, 8>
<5872, 68, 3>
<5872, 72, 8>
<5872, 80, 3>
<5872, 84, 8>
<5872, 92, 3>
<5872, 96, 8>
<5872, 104, 4>
<5872, 108, 8>
<5872, 116, 4>
ext4fs read 15 group descriptor (blkno 1 blkoff 480)
<8, 480, 32>
<3932176, 0, 128>
<3936200, 0, 8>
<3936200, 8, 1>
<3936200, 12, 8>
<3936200, 20, 2>
<3936200, 24, 8>
<3936200, 32, 40>
<3936200, 72, 8>
<3936200, 80, 40>
<3936200, 120, 8>
<3936200, 128, 6>
<3936200, 136, 8>
<3936200, 144, 23>
<3936200, 168, 8>
<3936200, 176, 21>
ext4fs read 15 group descriptor (blkno 1 blkoff 480)
<8, 480, 32>
<3932178, 256, 128>
Got symlink >devicetree-zImage-am57xx-beagle-x15.dtb<
ext4fs read 15 group descriptor (blkno 1 blkoff 480)
<8, 480, 32>
<3932176, 0, 128>
<3936200, 0, 8>
<3936200, 8, 1>
<3936200, 12, 8>
<3936200, 20, 2>
<3936200, 24, 8>
<3936200, 32, 40>
<3936200, 72, 8>
<3936200, 80, 40>
<3936200, 120, 8>
<3936200, 128, 6>
<3936200, 136, 8>
<3936200, 144, 23>
<3936200, 168, 8>
<3936200, 176, 21>
<3936200, 200, 8>
<3936200, 208, 22>
<3936200, 232, 8>
<3936200, 240, 14>
<3936200, 256, 8>
<3936200, 264, 14>
<3936200, 280, 8>
<3936200, 288, 39>
ext4fs read 15 group descriptor (blkno 1 blkoff 480)
<8, 480, 32>
<3932180, 256, 128>
<3940560, 0, 4096>
<4067328, 0, 65536>
<202880, 0, 21236>
86772 bytes read in 173 ms (489.3 KiB/s)
Initial value for argc=3
Final value for argc=3
Booting from mmc0 ...
Initial value for argc=3
Final value for argc=3
Initial value for argc=12
Final value for argc=12
## Current stack ends at 0xbef3ca40 * kernel: cmdline image address = 0x82000000
Kernel image @ 0x82000000 [ 0x000000 - 0x330c18 ]
## Skipping init Ramdisk
## No init Ramdisk
ramdisk start = 0x00000000, ramdisk end = 0x00000000
* fdt: cmdline image address = 0x88000000
## Checking for 'FDT'/'FDT Image' at 88000000
* fdt: raw FDT blob
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
of_flat_tree at 0x88000000 size 0x000152f4
Initial value for argc=3
Final value for argc=3
using: FDT
## initrd_high = 0xffffffff, copy_to_ram = 1
ramdisk load start = 0x00000000, ramdisk load end = 0x00000000
## device tree at 88000000 ... 880152f3 (len=99060 [0x182F4])
Loading Device Tree to 8ffe7000, end 8ffff2f3 ... OK
Initial value for argc=3
Final value for argc=3
## Transferring control to Linux (at address 82000000)...
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpuset
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 4.1.13-g8dc6617 (medha@medha) (gcc version 4.9.3 20150413 (prerelease) (Linaro GCC 4.9-2015.05) ) #7 SMP PREEMPT 6
[ 0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[ 0.000000] Machine model: TI AM571x IDK
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000095800000, size 56 MiB
[ 0.000000] Reserved memory: initialized node ipu2_cma@95800000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000099000000, size 64 MiB
[ 0.000000] Reserved memory: initialized node dsp1_cma@99000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x000000009d000000, size 32 MiB
[ 0.000000] Reserved memory: initialized node ipu1_cma@9d000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x000000009f000000, size 16 MiB
[ 0.000000] Reserved memory: initialized node dsp2_cma@9f000000, compatible id shared-dma-pool
[ 0.000000] cma: Reserved 24 MiB at 0x0000000094000000
[ 0.000000] Forcing write-allocate cache policy for SMP
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] DRA722 ES1.0
[ 0.000000] PERCPU: Embedded 11 pages/cpu @d3ab1000 s16128 r8192 d20736 u45056
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 129152
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=PARTUUID=00000000-02 rw mem=512M rootfstype=ext4 rootwait root=PARTUUID=000000t
[ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 312448K/521216K available (6263K kernel code, 287K rwdata, 2156K rodata, 328K init, 254K bss, 12160K reserved, 196608K )
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xe0800000 - 0xff000000 ( 488 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc0841074 (8421 kB)
[ 0.000000] .init : 0xc0842000 - 0xc0894000 ( 328 kB)
[ 0.000000] .data : 0xc0894000 - 0xc08dbc48 ( 288 kB)
[ 0.000000] .bss : 0xc08de000 - 0xc091d80c ( 255 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Additional per-CPU info printed with stalls.
[ 0.000000] RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.
[ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] OMAP clockevent source: timer1 at 32768 Hz
[ 0.000000] clocksource 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
[ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 65535999984741ns
[ 0.000000] OMAP clocksource: 32k_counter at 32768 Hz
[ 0.000396] Architected cp15 timer(s) running at 6.14MHz (virt).
[ 0.000396] clocksource arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idle_ns: 440795202250 ns
[ 0.000431] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns
[ 0.000442] Switching to timer-based delay loop, resolution 162ns
[ 0.000949] Console: colour dummy device 80x30
[ 0.000964] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.000971] This ensures that you still see kernel messages. Please
[ 0.000975] update your kernel commandline.
[ 0.000986] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
[ 0.000999] pid_max: default: 32768 minimum: 301
[ 0.001084] Security Framework initialized
[ 0.001120] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.001129] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.001656] Initializing cgroup subsys blkio
[ 0.001671] Initializing cgroup subsys memory
[ 0.001697] Initializing cgroup subsys devices
[ 0.001709] Initializing cgroup subsys freezer
[ 0.001720] Initializing cgroup subsys perf_event
[ 0.001742] CPU: Testing write buffer coherency: ok
[ 0.002016] /cpus/cpu@0 missing clock-frequency property
[ 0.002029] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.002062] Setting up static identity map for 0x800082c0 - 0x80008318
[ 0.040743] Brought up 1 CPUs
[ 0.040755] SMP: Total of 1 processors activated (12.29 BogoMIPS).
[ 0.040762] CPU: All CPU(s) started in SVC mode.
[ 0.041126] devtmpfs: initialized
[ 0.064260] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
[ 0.065074] omap_hwmod: l3_main_2 using broken dt data from ocp
[ 0.077968] omap_hwmod: tptc0 using broken dt data from edma-controller
[ 0.078417] omap_hwmod: tptc1 using broken dt data from edma-controller
[ 0.152122] omap_hwmod: dcan2: _wait_target_disable failed
[ 0.246116] clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.249296] ------------[ cut here ]------------
[ 0.249327] WARNING: CPU: 0 PID: 1 at mm/cma.c:117 cma_init_reserved_areas+0x144/0x218()
[ 0.249336] Modules linked in:
[ 0.249355] CPU: 0 PID: 1 Comm: swapper/0 Not tainted 4.1.13-g8dc6617 #7
[ 0.249363] Hardware name: Generic DRA72X (Flattened Device Tree)
[ 0.249370] Backtrace:
[ 0.249395] [<c0012f78>] (dump_backtrace) from [<c001319c>] (show_stack+0x18/0x1c)
[ 0.249402] r7:c085d51c r6:00000075 r5:c08b390c r4:00000000
[ 0.249432] [<c0013184>] (show_stack) from [<c061cdbc>] (dump_stack+0x9c/0xdc)
[ 0.249446] [<c061cd20>] (dump_stack) from [<c0039428>] (warn_slowpath_common+0x88/0xb8)
[ 0.249452] r5:00000009 r4:00000000
[ 0.249468] [<c00393a0>] (warn_slowpath_common) from [<c00394fc>] (warn_slowpath_null+0x24/0x2c)
[ 0.249474] r8:c08fe8ac r7:0009fd00 r6:c08d9680 r5:c08db47b r4:c08d9680
[ 0.249502] [<c00394d8>] (warn_slowpath_null) from [<c085d51c>] (cma_init_reserved_areas+0x144/0x218)
[ 0.249514] [<c085d3d8>] (cma_init_reserved_areas) from [<c00097a8>] (do_one_initcall+0x94/0x1e0)
[ 0.249520] r10:00000000 r9:c08425ec r8:c088e8a0 r7:d353d840 r6:c0899120 r5:c085d3d8
[ 0.249542] r4:c0899120
[ 0.249558] [<c0009714>] (do_one_initcall) from [<c0842f28>] (kernel_init_freeable+0x1d0/0x274)
[ 0.249564] r10:c08822bc r9:c08425ec r8:c088e8a0 r7:c08de000 r6:c08de000 r5:c08822a0
[ 0.249584] r4:00000001
[ 0.249598] [<c0842d58>] (kernel_init_freeable) from [<c0619458>] (kernel_init+0x18/0xf0)
[ 0.249603] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c0619440
[ 0.249623] r4:c08de000
[ 0.249636] [<c0619440>] (kernel_init) from [<c000fa08>] (ret_from_fork+0x14/0x2c)
[ 0.249642] r5:c0619440 r4:00000000
[ 0.249668] ---[ end trace 5dce64b5a7557113 ]---
[ 0.250410] pinctrl core: initialized pinctrl subsystem
[ 0.251309] NET: Registered protocol family 16
[ 0.252313] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.260479] OMAP GPIO hardware version 0.1
[ 0.266986] irq: no irq domain found for /ocp/l4@4a000000/scm@2000/pinmux@1400 !
[ 0.284710] No ATAGs?
[ 0.284735] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[ 0.284744] hw-breakpoint: maximum watchpoint size is 8 bytes.
[ 0.287192] omap4_sram_init:Unable to allocate sram needed to handle errata I688
[ 0.287202] omap4_sram_init:Unable to get sram pool needed to handle errata I688
[ 0.287772] OMAP DMA hardware revision 0.0
[ 0.328027] edma-dma-engine edma-dma-engine.0: TI EDMA DMA engine driver
[ 0.330787] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver
[ 0.335181] ------------[ cut here ]------------
[ 0.335204] WARNING: CPU: 0 PID: 1 at drivers/iommu/omap-iommu.c:1433 omap_iommu_add_device+0xd0/0x108()
[ 0.335211] Modules linked in:
[ 0.335225] CPU: 0 PID: 1 Comm: swapper/0 Tainted: G W 4.1.13-g8dc6617 #7
[ 0.335233] Hardware name: Generic DRA72X (Flattened Device Tree)
[ 0.335239] Backtrace:
[ 0.335261] [<c0012f78>] (dump_backtrace) from [<c001319c>] (show_stack+0x18/0x1c)
[ 0.335268] r7:c03b8a3c r6:00000599 r5:c08b390c r4:00000000
[ 0.335295] [<c0013184>] (show_stack) from [<c061cdbc>] (dump_stack+0x9c/0xdc)
[ 0.335308] [<c061cd20>] (dump_stack) from [<c0039428>] (warn_slowpath_common+0x88/0xb8)
[ 0.335314] r5:00000009 r4:00000000
[ 0.335331] [<c00393a0>] (warn_slowpath_common) from [<c00394fc>] (warn_slowpath_null+0x24/0x2c)
[ 0.335336] r8:00000002 r7:ffffffea r6:d3615b00 r5:d3615b00 r4:00000000
[ 0.335362] [<c00394d8>] (warn_slowpath_null) from [<c03b8a3c>] (omap_iommu_add_device+0xd0/0x108)
[ 0.335375] [<c03b896c>] (omap_iommu_add_device) from [<c03b7040>] (add_iommu_group+0x34/0x54)
[ 0.335380] r9:c08425ec r8:c088ea50 r7:d36159c0 r6:c03b700c r5:c0668ea0 r4:d35a1210
[ 0.335409] [<c03b700c>] (add_iommu_group) from [<c03fed70>] (bus_for_each_dev+0x70/0xa4)
[ 0.335415] r5:d346be94 r4:00000000
[ 0.335432] [<c03fed00>] (bus_for_each_dev) from [<c03b7760>] (bus_set_iommu+0x84/0xc8)
[ 0.335437] r6:d36159c0 r5:00000000 r4:c08c1ab0
[ 0.335455] [<c03b76dc>] (bus_set_iommu) from [<c086ae0c>] (omap_iommu_init+0x78/0x98)
[ 0.335461] r6:c0899120 r5:c086ad94 r4:c0899120
[ 0.335478] [<c086ad94>] (omap_iommu_init) from [<c00097a8>] (do_one_initcall+0x94/0x1e0)
[ 0.335490] [<c0009714>] (do_one_initcall) from [<c0842f28>] (kernel_init_freeable+0x1d0/0x274)
[ 0.335496] r10:c08822bc r9:c08425ec r8:c088ea50 r7:c08de000 r6:c08de000 r5:c08822ac
[ 0.335517] r4:00000004
[ 0.335530] [<c0842d58>] (kernel_init_freeable) from [<c0619458>] (kernel_init+0x18/0xf0)
[ 0.335536] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c0619440
[ 0.335555] r4:c08de000
[ 0.335567] [<c0619440>] (kernel_init) from [<c000fa08>] (ret_from_fork+0x14/0x2c)
[ 0.335573] r5:c0619440 r4:00000000
[ 0.335584] ---[ end trace 5dce64b5a7557114 ]---
[ 0.336078] omap-iommu 40d02000.mmu: 40d02000.mmu registered
[ 0.336245] omap-iommu 58882000.mmu: 58882000.mmu registered
[ 0.336396] omap-iommu 55082000.mmu: 55082000.mmu registered
[ 0.336670] vgaarb: loaded
[ 0.337021] SCSI subsystem initialized
[ 0.338146] palmas 0-0058: Irq flag is 0x00000000
[ 1.351619] omap_i2c 48070000.i2c: timeout waiting for bus ready
[ 1.351633] palmas 0-0058: POLARITY_CTRL updat failed: -110
[ 1.351940] palmas: probe of 0-0058 failed with error -110
[ 1.352063] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
[ 1.352230] media: Linux media interface: v0.10
[ 1.352285] Linux video capture interface: v2.00
[ 1.352328] pps_core: LinuxPPS API ver. 1 registered
[ 1.352334] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 1.352360] PTP clock support registered
[ 1.352983] omap-mailbox 4883c000.mailbox: omap mailbox rev 0x400
[ 1.353268] omap-mailbox 4883e000.mailbox: omap mailbox rev 0x400
[ 1.353550] omap-mailbox 48840000.mailbox: omap mailbox rev 0x400
[ 1.353619] omap-mailbox: probe of 48842000.mailbox failed with error -22
[ 1.353845] Advanced Linux Sound Architecture Driver Initialized.
[ 1.354519] Switched to clocksource arch_sys_counter
[ 1.364191] NET: Registered protocol family 2
[ 1.364795] TCP established hash table entries: 4096 (order: 2, 16384 bytes)
[ 1.364835] TCP bind hash table entries: 4096 (order: 3, 32768 bytes)
[ 1.364901] TCP: Hash tables configured (established 4096 bind 4096)
[ 1.364943] UDP hash table entries: 256 (order: 1, 8192 bytes)
[ 1.364964] UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
[ 1.365142] NET: Registered protocol family 1
[ 1.365392] RPC: Registered named UNIX socket transport module.
[ 1.365401] RPC: Registered udp transport module.
[ 1.365408] RPC: Registered tcp transport module.
[ 1.365414] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 1.366413] CPU PMU: Failed to parse /pmu/interrupt-affinity[0]
[ 1.366444] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available
[ 1.368338] futex hash table entries: 256 (order: 2, 16384 bytes)
[ 1.368409] audit: initializing netlink subsys (disabled)
[ 1.368448] audit: type=2000 audit(1.350:1): initialized
[ 1.375559] VFS: Disk quotas dquot_6.6.0
[ 1.375712] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 1.377674] NFS: Registering the id_resolver key type
[ 1.377710] Key type id_resolver registered
[ 1.377717] Key type id_legacy registered
[ 1.377776] jffs2: version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc.
[ 1.380121] NET: Registered protocol family 38
[ 1.380168] io scheduler noop registered
[ 1.380180] io scheduler deadline registered
[ 1.380218] io scheduler cfq registered (default)
[ 1.383720] pinctrl-single 4a003400.pinmux: 281 pins at pa fc003400 size 1124
[ 1.383833] pinctrl-single 4a002e8c.pinmux: 1 pins at pa fc002e8c size 4
[ 1.417169] dra7-pcie 51000000.pcie: PCI host bridge to bus 0000:00
[ 1.417183] pci_bus 0000:00: root bus resource [io 0x1000-0xffff]
[ 1.417194] pci_bus 0000:00: root bus resource [mem 0x20013000-0x2fffffff]
[ 1.417204] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 1.417326] pci 0000:00:00.0: IOMMU is currently not supported for PCI
[ 1.417594] PCI: bus0: Fast back to back transfers disabled
[ 1.417722] PCI: bus1: Fast back to back transfers enabled
[ 1.417819] pci 0000:00:00.0: BAR 0: assigned [mem 0x20100000-0x201fffff]
[ 1.417833] pci 0000:00:00.0: BAR 1: assigned [mem 0x20020000-0x2002ffff]
[ 1.417845] pci 0000:00:00.0: PCI bridge to [bus 01]
[ 1.419564] omapdss_dss 58000000.dss: master bind failed: -517
[ 1.421430] tlc59108 0-0040: failed to find video source
[ 1.423946] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[ 1.426920] 4806a000.serial: ttyS0 at MMIO 0x4806a000 (irq = 299, base_baud = 3000000) is a 8250
[ 2.743058] console [ttyS0] enabled
[ 2.747225] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 300, base_baud = 3000000) is a 8250
[ 2.757061] [drm] Initialized drm 1.1.0 20060810
[ 2.769969] brd: module loaded
[ 2.777162] loop: module loaded
[ 2.781198] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 2.834539] davinci_mdio 48485000.mdio: davinci mdio revision 1.6
[ 2.840663] davinci_mdio 48485000.mdio: detected phy mask fffffdff
[ 2.849246] libphy: 48485000.mdio: probed
[ 2.853277] davinci_mdio 48485000.mdio: phy[9]: device 48485000.mdio:09, driver unknown
[ 2.861962] cpsw 48484000.ethernet: Detected MACID = 5c:f8:21:41:06:86
[ 2.869301] cpsw 48484000.ethernet: cpsw: Detected MACID = 5c:f8:21:41:06:87
[ 2.877674] mousedev: PS/2 mouse device common for all mice
[ 2.883326] i2c /dev entries driver
[ 2.888885] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 2.893754] omap_hsmmc 4809c000.mmc: no pinctrl state for sdr104 mode
[ 2.900284] omap_hsmmc 4809c000.mmc: no pinctrl state for ddr50 mode
[ 2.906703] omap_hsmmc 4809c000.mmc: no pinctrl state for sdr50 mode
[ 2.913086] omap_hsmmc 4809c000.mmc: no pinctrl state for sdr25 mode
[ 2.919484] omap_hsmmc 4809c000.mmc: no pinctrl state for sdr12 mode
[ 2.925877] omap_hsmmc 4809c000.mmc: no pinctrl state for hs mode
[ 2.965156] omap_hsmmc 480b4000.mmc: no pinctrl state for default mode
[ 2.994815] ledtrig-cpu: registered to indicate activity on CPUs
[ 3.001147] omap-aes 4b500000.aes: OMAP AES hw accel rev: 3.3
[ 3.007760] omap-aes 4b700000.aes: OMAP AES hw accel rev: 3.3
[ 3.014041] omap-des 480a5000.des: OMAP DES hw accel rev: 2.2
[ 3.020896] omap-sham 4b101000.sham: hw accel on OMAP rev 4.3
[ 3.030120] oprofile: using timer interrupt.
[ 3.034436] mmc0: host does not support reading read-only switch, assuming write-enable
[ 3.042812] Initializing XFRM netlink socket
[ 3.047272] mmc0: new SDHC card at address 1234
[ 3.052117] NET: Registered protocol family 17
[ 3.056725] mmcblk0: mmc0:1234 SA04G 3.63 GiB
[ 3.061497] NET: Registered protocol family 15
[ 3.066253] Key type dns_resolver registered
[ 3.070611] mmcblk0: p1 p2
[ 3.073857] omap_voltage_late_init: Voltage driver support not added
[ 3.080869] Power Management for TI OMAP4+ devices.
[ 3.086053] ThumbEE CPU extension supported.
[ 3.090355] Registering SWP/SWPB emulation handler
[ 3.096665] dmm 4e000000.dmm: workaround for errata i878 in use
[ 3.104069] dmm 4e000000.dmm: initialized all PAT entries
[ 3.110240] omapdss_dss 58000000.dss: master bind failed: -517
[ 3.116446] tlc59108 0-0040: failed to find video source
[ 3.122126] hctosys: unable to open rtc device (rtc0)
[ 3.139043] vdd_3v3: disabling
[ 3.142324] ALSA device list:
[ 3.145340] No soundcards found.
[ 3.178233] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 3.186452] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 3.197921] devtmpfs: mounted
[ 3.201112] Freeing unused kernel memory: 328K (c0842000 - c0894000)
INIT: version 2.88 booting
Error opening /dev/fb0: No such file or directory
Starting udev
[ 5.182661] udevd[96]: starting version 182
[ 5.511051] debugss_kmodule: disagrees about version of symbol module_layout
[ 5.637966] debugss_kmodule: disagrees about version of symbol module_layout
[ 5.795503] omap_rng 48090000.rng: OMAP Random Number Generator ver. 20
[ 5.802452] omapdss_dss 58000000.dss: master bind failed: -517
[ 5.837280] tlc59108 0-0040: failed to find video source
[ 6.059859] omap_rtc 48838000.rtc: rtc core: registered 48838000.rtc as rtc0
[ 6.174652] omapdss_dss 58000000.dss: master bind failed: -517
[ 6.180848] tlc59108 0-0040: failed to find video source
[ 6.196809] vpe 489d0000.vpe: loading firmware vpdma-1b8.bin
[ 6.274804] vpe 489d0000.vpe: Device registered as /dev/video0
[ 6.316289] omapdss_dss 58000000.dss: master bind failed: -517
[ 6.323663] tlc59108 0-0040: failed to find video source
[ 6.389050] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 6.451257] omapdrm_pvr: disagrees about version of symbol module_layout
[ 6.498564] extcon-usb-gpio extcon_usb1: failed to get ID GPIO
[ 6.504434] extcon-usb-gpio: probe of extcon_usb1 failed with error -2
[ 6.564122] omapdrm_pvr: disagrees about version of symbol module_layout
[ 6.595112] omapdss_dss 58000000.dss: master bind failed: -517
[ 6.602518] tlc59108 0-0040: failed to find video source
[ 6.661005] extcon-usb-gpio extcon_usb2: failed to get ID GPIO
[ 6.834740] extcon-usb-gpio: probe of extcon_usb2 failed with error -2
[ 7.450327] m25p80 spi32766.0: unrecognized JEDEC id bytes: 00, 0, 0
[ 7.898293] cmemk: disagrees about version of symbol module_layout
[ 7.933729] cryptodev: disagrees about version of symbol module_layout
[ 7.963072] gdbserverproxy: disagrees about version of symbol module_layout
[ 7.996574] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
bootlogd: cannot allocate pseudo tty: No such file or directory
Starting random number generator daemon.
[ 8.099364] random: nonblocking pool is initialized
ALSA: Restoring mixer settings...
/usr/sbin/alsactl: load_state:1729: No soundcards found...
Sat Jan 9 01:21:27 UTC 2016
INIT: Entering runlevel: 5
Configuring network interfaces... [ 28.894620] net eth0: initializing cpsw version 1.15 (0)
[ 28.902933] libphy: PHY 48485000.mdio:02 not found
[ 28.907977] net eth0: phy 48485000.mdio:02 not found on slave 0
udhcpc (v1.23.1) started
Sending discover...
Sending discover...
Sending discover...
No lease, forking to background
done.
Starting system message bus: dbus.
UIM SYSFS Node Not Found
Initializing the graphics driver ...
PVR:(Error): OpenServices: drmOpen failed [120, /pvr_bridge_u.c]
PVR:(Error): PVRSRVInitSrvConnect: PVRSRVConnect failed [2572, /bridged_pvr_glue.c]
PVR:(Error): SrvInit: PVRSRVInitSrvConnect failed (4) [37, /srvinit.c]
PVR:(Error): main: SrvInit failed (4) [47, /pvrsrvinit.c]
Starting Dropbear SSH server: Generating key, this may take a while...
Public key portion is:
ssh-rsa AAAAB3NzaC1yc2EAAAADAQABAAABAQDq8021k+SN2nI+Iqq57i/1LbpC2TxZtlSaPjUiVgKFWkO3enVn5nSJ0RGs5RzsEDkKkso0dVkhPBz69Qi7VNyMUZApxrLiYR2XntgqhVm
Fingerprint: md5 ab:3c:e2:26:52:3a:bf:bb:53:ed:e4:4c:f1:1e:58:e6
[ 42.056737] NET: Registered protocol family 10
[ 42.064988] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
dropbear.
Starting telnet daemon.
Starting tiipclad daemon
GateMP support enabled on host
Opened log file: lad.txt
numProcessors = 5 id = 0 baseId = 0
Spawned daemon: /usr/bin/lad_dra7xx
.
Starting rpcbind daemon...done.
starting statd: done
Starting syslogd/klogd: done
Starting thttpd.
[ ok ]rting Avahi mDNS/DNS-SD Daemon: avahi-daemon
Starting Telephony daemon
Starting Lighttpd Web Server: lighttpd.
2000-01-01 00:00:00: (/home/gtbldadm/processor-sdk-linux-fido-build/build-CORTEX_1/arago-tmp-external-linaro-toolchain/work/cortexa15hf-vfp-ne
/
Starting Matrix GUI application.
Enabling thermal zones...
***************************************************************
***************************************************************
NOTICE: This file system contains the following GPLv3 packages:
autoconf
binutils-dev
binutils
bison-dev
bison
coreutils-dev
coreutils
cpp-symlinks
cpp
g++-symlinks
g++
gawk-dev
gawk
gcc-symlinks
gcc
gdb
gdbc6x
gdbserver
gstreamer1.0-libav
libgmp-dev
libgmp10
libgmpxx4
libmpc3
libmpfr4
make
parted
swig-dev
swig
If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
The log is same up to starting kernel when hangs at starting kernel. I dont think it is because of different UART interfaces difference in u-boot and kernel. Any suggestion for debugging this problem?