This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/AM3352: Package ti.ndk.config not located

Part Number: AM3352

Tool/software: Code Composer Studio

I am using CCS 6.1 on Windows 7. I just downloaded and installed the RTOS SDK: http://www.ti.com/.../PROCESSOR-SDK-AM335X, and when I attempt to build my project, i receive the following error:

xdc.services.global.XDCException: xdc.PACKAGE_NOT_FOUND: can't locate the package 'ti.ndk.config' along the path: 'C:/ti/bios_6_46_01_38/packages;C:/ti/ccsv6/ccs_base;C:/ti/xdctools_3_32_01_22_core/packages;..;'. Ensure that the package path is set correctly.

I looked for a ti.ndk.config file, and I found these files in C:\ti\ndk_2_25_00_09\packages\ti\ndk\config\package:

package_ti.ndk.config.c
ti.ndk.config.ccs
ti.ndk.config.sch

Can someone help resolve this?

  • Hi George,

    Do you have the NDK selected in the Project Properties->General->RTSC window? If not, check the 2.25.00.09 version product. If you don't see it, go to Window->Preferences->Code Composer Studio->RTSC->Product and do a "Search Now" if you have the NDK in c:\ti, it will find it. After you install it and restart CCS, you can then check 2.25.00.09 in the project properties.

    Todd

    Todd
  • There was a suggested answer and since there has been no active on this thread for more than a week, the suggested answer was marked as verify. Please feel free to select the "Reject Answer" button and reply with more details.