Part Number: TMS320C6657
Hello,
Could you tell me what value I should enter for CorePac Util in Power Spreadsheet (Excel)? In my application, the time ratio of CPU utilization is SP=40%, CC=40% and IDLE=20% roughly. SP has 4 parallel instructions on average which are half of 8 parallels. I guess I should not set SP to 40%. Please tell me what value I should enter to SP and CC.
The application note (SPRABI5A) has the following description.
% Signal Processing (SP) Utilization is used to represent scenarios with high levels of DSP activity. This corresponds to the case in which all eight instructions fetched by the DSP are executed in parallel each DSP clock cycle, resulting in all eight functional units being active every cycle.
Regards,
Kazu