Part Number: DM3725
Hi,
I am implementing eHCILL protocol on DM3725 for BT which is having wilink-8 chip.
Now I want to understand that If I want interrupt of the CTS pin of UART-2 then what is the procedure for that ?
If I configure CTS pin into GPIO and then try configuring interrupt on this pin then what can be the procedure.
What is the main difference between above two scenario
Regards,
Abhi