Part Number: TMS320DM8168
Other Parts Discussed in Thread: SYSCONFIG
Hi,
Following is a summary of the boot issue observed by us. I would be grateful to receive some inputs from TI to resolve this.
1. DM816x is configured to NAND Boot. BTMODE[3:0] = 10010 (Value of Boot Stat register is 20312). This processor Board connects to another FPGA board (Xilinx FPGA) and the mode of communication with FPGA is the GPMC interface (control signals, address[16:1] and Data bus[15:0]).
2. The DM816x board boots up when it is standalone. But when it is connected to FPGA board which is powered ON it does not boot from NAND.
3. All the IOs on the FPGA corresponding to the GPMC signals including the bootmode are in tristated condition and there are no external Pull-ups or Pull-downs on the FPGA board.
4. In the state of not being able to boot, the CCS connection was establised and the RBL tracing vectors registers were read which point to the fact that NAND boot is failing and the device is going to UART boot, (which we are able to observe on the console with prints coming on UART0). The Program Counter in CCS also points to the address in RBL address range.
Please share some inputs on what might be causing the NAND Boot to fail.
Regards,
Shareef