This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/CC3200-LAUNCHXL: Why can i not call funtions by the // Macros for the ADC API.???????

Part Number: CC3200-LAUNCHXL


Tool/software: TI-RTOS

I cannot call for these functions from the empty.c 

MAP_ADCTimerEnable(ADC_BASE);
MAP_ADCChannelEnable(ADC_BASE, ADC_CH_1);
ulSample = MAP_ADCFIFORead(ADC_BASE, uiChannel);
MAP_ADCChannelDisable(ADC_BASE, uiChannel);

when i check the linking i reach to "rom_map.h" but thereafter i see this error.

Selected text cannot be mapped to a symbol name.

is there some missing links that I need to make manually.???