Other Parts Discussed in Thread: AM5728
Tool/software: Linux
Hi,
TI,
Does the dts support two rx configuration in the serial-dir?There is a adau1978 sound codes connects to the mcasp6 of am5728 like that:
the mcasp6_axr0 and mcasp6_axr1 are work on the rx mode too.
There are four line input on the adau1978.The data of input0 and input1 will output to the mcasp6_axr0,and the The data of input2 and input3 will output to the mcasp6_axr1.
I use "arecord -Dhw:0,0 -f S16_LE -r 44100 -d 10 -c 2 1.wav" to record,and I can get the data of input0 and input1,but not the input2 and input3.After modify the dts file like that,then I can get the data of input2 and input3,but not the input0 and input1.
It seems that if I configurate two rx pins,only the first rx pins can work.
Any ideas?
Thank you!
BR,
vefone