Part Number: TMS320DM8148
Hi All,
Please find below basic info:
Processor : TMS320DM8148
EZSDK version : ezsdk_5_05_02_00
Linux kernel version : linux-2.6.37-psp04.04.00.01
Syslink version : syslink_2_20_02_20
In our project we are using Ittiam provided audio encoder which is codec engine API based implementation.
It contains sample application for audio encoding.
This application is running fine. But not always. Sometimes at exit of an application there is large carsh coming at the end.
Crash show that it is coming from syslink driver.
CPU: 0 Not tainted (2.6.37-centaurus-036 #1)
PC is at _TransportShm_notifyFxn+0xac/0xfc [syslink]
LR is at MessageQ_put+0x478/0x4e4 [syslink]
pc : [<bf09f334>] lr : [<bf082b30>] psr: 80000013
sp : c5967e38 ip : 00000000 fp : c5967e5c
r10: 00000004 r9 : c054e934 r8 : 00000002
r7 : cb805a80 r6 : 00000000 r5 : cbf2c000 r4 : cb807480
r3 : 00000000 r2 : 00000000 r1 : 00060000 r0 : 00000000
Flags: Nzcv IRQs on FIQs on Mode SVC_32 ISA ARM Segment kernel
Control: 10c5387d Table: 85bf4019 DAC: 00000017
Process kworker/0:1 (pid: 22, stack limit = 0xc59662e8)
Due to this crash board hangs after that only power cycle reboot is an option. This issue is very critical.
Please find the attached crash log for your reference.
We are clueless about this issue and not sure how to debug this issue.
Any pointers or help regarding this issue will be appreciated. Let me know if any logs or more information is needed.
Thanks,
Jemish