I have some questions regarding dynamic power managment on C6472
- When a certain core of C6472 is in power sleep mode, is the core completely turned off or the core is just in sleep mode with low CPU usages?
- If the cores (especially all cores) are turned OFF or in sleep mode, I belive it would need external event to wake these up. What mechanism could we use to wake these up? Is it Interrupt? Is the interrupt controller still active in sleep mode? If not what could we use?
- Are there example projects to look into the code for setting up sleep and subsequent wakup for C6472? I am looking for example beyond just the document (SPRUEG3B.pdf)
Thanks,
Binh Vu