Hi,
I am using dm365EVM.
I want to encode the voice by using microphone input (M1) in EVM.
I completed the integration of MP3 codecs. (Refer to the following site)
http://processors.wiki.ti.com/index.php/DM365_Audio_Codecs_Integration_with_DVSDK_2.10.01.18_Demos
So , I can encode the voice via MIC IN (and LINE IN).
But, I do not know the setting method of M1.
What should I change to use M1? device driver ? application ?