Part Number: AM5728
Tool/software: Linux
Hello,
I am trying to build a linux pacakge for am5728 (Phytech-AM57xx), but I am getting error.
when I run "MACHINE=am57xx-phycore-rdk bitbake arago-core-tisdk-image" command
I got the following error :
ERROR: nativesdk-qtbase-5.6.0+gitAUTOINC+cec15a89d0-r0 do_compile: oe_runmake failed
ERROR: nativesdk-qtbase-5.6.0+gitAUTOINC+cec15a89d0-r0 do_compile: Function failed: do_compile (log file is located at /opt/PHYTEC_BSPs/yocto_ti/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.6.0+gitAUTOINC+cec15a89d0-r0/temp/log.do_compile.15714)
ERROR: Logfile of failure stored in: /opt/PHYTEC_BSPs/yocto_ti/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.6.0+gitAUTOINC+cec15a89d0-r0/temp/log.do_compile.15714
However, there were other errors that I resolved in the past, now I am blocked at this point.
Please let me know what could I do to avoid this because I do not find and link to download the missing packages online, and copy to download directory with the .done file creation.
Thanks in advance,
Regards,