Hi Folks,
The UG says "The resulting 8-bit sample data for each of the
enabled channels is then OR'd together to create a single 8-bit sample value that is
written to the appropriate transmit data register (DXn). The ability to combine the data
from multiple channels enables the creation and use of physical timeslot sharing
provided that the bit values are zero for the unused bits in the physical timeslot data for
a given channel. "
Could you please describe easily?
I can not figure out the relationship among the procedures DX/DR <-> Channel Buffer <-> DSP internal RAM with Bitmap context.
Thank you very much for your time to explanation.
Best regards,
Hitoshi