Hi,
can i run av_server ipnc application in a NFS filesystem?
if i try to load it i obtain this output
root@10.0.0.2:/opt/ipnc# ./av_capture_load.sh
cmemk unregistered
irqk unregistered
CSL: Module install successful, device major num = 253
CSL: Module version 0.10.00, built on Jul 23 2010 15:46:06
I2C: Module install successful, device major num = 252
DMA: Module install successful, device major num = 251
DRV: Module install successful
DRV: Module built on Jul 23 2010 15:46:13
DRV: EDMACC.QUEPRI = 00000777
DRV: SYSTEM.MSTPRI0 = 00550011
DRV: SYSTEM.MSTPRI1 = 00000444
DRV: ISP.BCR = 00000002
CMEMK module: built on Jul 23 2010 at 15:45:16
Reference Linux version 2.6.18
File /home/software/dvsdk_2_10_01_18/linuxutils_2_24_03/packages/ti/sdo/linuxutils/cmem/src/module/cmemk.c
allocated heap buffer 0xc5000000 of size 0x4800000
CMEM Range Overlaps Kernel Physical - allowing overlap
CMEM phys_start (0x1000) overlaps kernel (0x80000000 -> 0x83800000)
cmemk initialized
EDMAK module: built on Jul 23 2010 at 15:45:21
Reference Linux version 2.6.18
File /home/software/dvsdk_2_10_01_18/linuxutils_2_24_03/packages/ti/sdo/linuxutils/edma/src/module/edmak.c
IRQK module: built on Jul 23 2010 at 15:45:23
Reference Linux version 2.6.18
File /home/software/dvsdk_2_10_01_18/linuxutils_2_24_03/packages/ti/sdo/linuxutils/irq/src/module/irqk.c
irqk initialized
root@10.0.0.2:/opt/ipnc# ./loadmodules_ipnc.sh
sbulla: unknown partition table
mkdosfs 2.11 (12 Mar 2005)
unable to get drive geometry, using default 255/63/dev/sbulla has 255 heads and 63 sectors per track,
logical sector size is 512,
using 0xf8 media descriptor, with 1024 sectors;
file system has 2 12-bit FATs and 4 sectors per cluster.
FAT size is 1 sector, and provides 247 clusters.
Root directory contains 512 slots.
Volume ID is 386daa72, no volume label.
root@10.0.0.2:/opt/ipnc# ./system_server &
[1] 1409
root@10.0.0.2:/opt/ipnc# queue id:0
Creat queue id:131075
queue id:131075
IPNC_1.5 (software@software-desktop) (gcc version 4.2.0 (MontaV
queue id:65537
queue id:131075
FileMng: Error Can't create system file
Kill queue id:131075
queue id:65537
FileMsgDrv: Error
Data read error
FileMsgDrv: Error
Data read error
Can't get system info!!
FileMsgDrv: Error
Data read error
Have i to modify something? What could be wrong?
Regards
Andrea