This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6678: TSIP "pending active" condition

Part Number: TMS320C6678

Hi Champs,

2.6.1 Transmit and Receive Channel Context
A channel configuration (A or B) that is pending active also is write protected.

Could you let me know what "pending active" means?

Best regards,
Hitoshi



  • I've forwarded this to the RSIP experts. Their feedback should be posted here.

    BR
    Tsvetolin Shulev
  • Hi,

    When a channel configuration (A or B) is active those configuration

    registers are write protected. A channel configuration (A or B) that is pending active

    also is write protected. Write accesses to the inactive configuration registers update the

    inactive registers.

    When the channel is disabled both bitmaps are inactive and can be modified. The least

    significant bit of the CnID value determines which of the two channel bitmaps is made

    pending and becomes active on the next superframe. A channel bitmap can be

    designated as pending active at any time. When a bitmap becomes pending active, both

    it and the active bitmap are protected until the pending active bitmap is made active

    and the active bitmap is made inactive. Changes in the actual active assignment always

    occur on a superframe.

    Pending active means you will be active in the next superframe. What is current active will be inactive in the next superframe.

    Regards, Eric