This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3351: Memory and low power state questions

Part Number: AM3351

questions from field:

1. Does AM3351/54 support MCP memory ? MCP is combined LPDDR+eMMC package. Ex part number is H9TQ64A8GTBCUR from Hynix.

2. What are low power states supported by AM3351/54? Application is running on batteries and when it is not in use, it has to be lowest power state, but should be able to wake up in couple of hundred ms with any interrupts like notification thru wifi/ user picking up remote/ button press etc. 

3. Do you have any comparison of power consumption in the system with DDR3 vs LPDDR for similar use cases? 

4. The LPDDR mentioned in spec, is it LPDDR1 only? Does not work with LPDDR2/3?

5. Power consumption in low power state.

6. For Mic In and 1W speaker out, do we need to have external audio Codec?

7. Any of the proposed PMIC support fuel gauge feature?