Part Number: DRA72XEVM
Tool/software: Linux
I want to run weston with the ivi-shell,how can I configue the weston.ini?And what dynamic library would be linked when the weston is running?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DRA72XEVM
Tool/software: Linux
I want to run weston with the ivi-shell,how can I configue the weston.ini?And what dynamic library would be linked when the weston is running?
Hi Zang,
You can try with attached weston.ini for ivi-shell. It uses weston's hmi-controller.so as ivi-controller.
HI Ramprasad :
I appreciate you that respond me soon.
dra7xx-evm login: root root@dra7xx-evm:~# pvrsrvinit root@dra7xx-evm:~# weston --tty=1 --idle-time=0 Date: 2017-01-20 UTC [06:35:36.328] weston 1.6.0 http://wayland.freedesktop.org/ Bug reports to: https://bugs.freedesktop.org/enter_bug.cgi?product=Wayland&component=weston&version=1.6.0 Build: 1.5.93-5-g2858cc2 configure.ac: bump version to 1.6.0 (2014-09-19 13:40:14 +0300) [06:35:36.328] OS: Linux, 3.14.63, #1 SMP PREEMPT Tue Jan 17 11:15:25 CST 2017, armv7l [06:35:36.329] Using config file '/etc//weston.ini' [06:35:36.331] Loading module '/usr/lib/weston/wayland-backend.so' [06:35:36.382] failed to create display: No such file or directory [06:35:36.382] fatal: failed to create compositor root@dra7xx-evm:~#