Tool/software: TI-RTOS
Hi
I was unable to run my application, based on TI RTOS version "tirtos_tivac_2_16_01_14", without debugging. After much debugging I found that its reason is HTTPS task. I then tested the HTTPs Client example. I have modified the example to get the data on the UART instead of IDE Terminal via semi-hosting. This example shows the same behavior. I can get data from the server in debug mode, but not without debugging.
I have attached the HTTPs file example. Can you please look at it to see what is needed to run HTTPS Client without debugging.
Edit: I am using UART 7 on Tiva Launch pad 129XL to get the debug information.
File: