Hi,
Actually I managed to write a piece of code for initializing the HPI.
My first test is to try to read the HPIC reg but it doesn't seem to work so well.
I have a quite simple question to start with :
Does /HPI_READY need a pull-up resistor ?
if yes is it possible to use an internal pull-up ?
rem : I tagged 6747 UHPI although I'm working on a C6748 but since it's the closest one... [ed: fixed]