This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6678: PCIe outbound payload size with EDMA

Part Number: TMS320C6678


For the PCIe outbound transfer, if using EDMA3 CC0 with TC0 or TC1, the data payload in the TLP is 64 bytes that is not equal to the data burst size (DBS) of the EDMA transfer controller (TC), if using EDMA3 CC1 with TC0, the data payload in the TLP is 128 bytes that is equal to the data burst size (DBS) of the EDMA transfer controller (TC).
Why the data payload is 64 bytes that is not equal to the DBS when using EDMA3 CC0?
Best regards,
Daisuke