This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320DM365: USB host implementation issue

Part Number: TMS320DM365


Dear Champs,

My customer wants to use USB port as HOST mode only, and they pull-down USB_ID pin(M1) with 1.5K ohm resistor as mentioned in datasheet.

But, they found their board recognized as device mode at sometime although they pull-down USB_ID pin(M1).

Can you guess why this device mode detection was occurred at sometime?

Do you think this can be caused by their charge pump design on VBUS?

I found charge pump should be used to supply 5V on VBUS on below e2e.

Is there anything else they should do to make sure USB HOST mode on DM365?

Thanks and Best Regards,

SI.