This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM3352: ALE Supervisory Packets

Part Number: AM3352

Tool/software: Linux

Hello

I don't understand of function of "Supervisory Packet" of am335x's ALE function, that is explanded at 14.3.2.7.1.2 "multicast Address Table Entry in TI's TRM.

Thank you for reading my question.

  • Hi,

    The Ethernet experts have been notified. They will respond here.
  • In the lead in section 14.3.2.7 Address Lookup Engine (ALE), at the end of the section there is a paragraph that describes what a supervisory packet is for both multicast and unicast. Essentially is saying that an address can be exempted from rate limiting by setting the supervisory bit for the entry in the ALE.

    "Multicast supervisory packets are designated by the super bit in the table entry. Unicast supervisory
    packets are indicated when block and secure are both set. Supervisory packets are not dropped due to
    rate limiting, OUI, or VLAN processing."