This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/PROCESSOR-SDK-AM335X: LTP-DDT dependencies

Part Number: PROCESSOR-SDK-AM335X

Tool/software: Linux

We are using Yocto to build our customized ROOTFS. On top of it, we installed LTP-DDT and tred to run DDT tests like MMC/eMMC/USB. Unfortunately all DDT tests tests are getting exited with error
++++++++++++++++++++++++++++++++++++
losetup failed to create block device
no block device was specified on commandline.
Block device could not be created using loopback device
Tests which require block device are disabled.
+++++++++++++++++++++++++++++++



But tests are running successfully when I used ROOTFS from TISDK release. It seems during the ROOTFS customization, few packages are missing. Can someone list the mandatory rootfs packages needed for LTP-DDT.



Thanks & Regards,

Ramakrishna